Skip to main content
Visitor II
April 2, 2024
Question

About VL53L4CX -Getting the best single-target data

Hi,

I have two questions to ask.

1、How do I adjust "VL53LX_MAX_RANGE_RESULTS"and "VL53LX_MAX_USER_ZONES"

if I want to get a best single target of data?

Would it be better to change them all to 1? It's not in the manual.

2、VL53L1CB has a single-target get function "SetSimpleData" that I can't find in the L4CX API. Are there any other functions that can help determine this?

Thanks.

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
April 22, 2024

The user API that is documented is the file vl53lx_api.c. The files in the vl53lx_api_core.c file were really not meant to be called by the user. 

Neither of those parameters are going to help you get the best single target. 

MAX_RANGE_RESULTS

if you ask for 2 targets you will get a distance to an object and the distance to the wall behind the target. 

if you ask for only 1 target, you can get either the strongest signal or the closest. It depends on what you want.

MAX_USER_ZONES

Each range you get the opportunity to change the region of interest. By taking a sub-sample of the full SPAD photon detection array, you and perhaps find more information. But this only makes sense if you use the VL53L1CD as it has a lens over the receive side of the sensor. That code is a remnant of the prior sensor. 

The VL53LX is a VL53L1CB with the lens removed. Turns out that lens is pretty costly. 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
GHuan.2
Associate II
February 28, 2025

Hi John, I have the same question for VL53L3CX. After reading your reply last April, my understanding is that for VL53L3CX, we need to set VL53LX_MAX_USER_ZONES to 1, and set VL53LX_MAX_RANGE_RESULTS to 1 or 2, as my application needs, right? Besides i want to save some ram with my app.