Skip to main content
DSai.1
Associate III
July 23, 2022
Solved

About driver for VL53L1X

Dear Sir,

​

We will develop system with VL53L1X. Now we are going to port the driver for our Thread RTOS. There are several sample version at candidates such as STSW-IMG007

, STSW-IMG009 , STSW-IMG013 and STSW-IMG032. Could you give me some advice for selecting the sample code? which one is better for our case?

best regards

Dai Sai

This topic has been closed for replies.
Anne BIGOT
Anne BIGOTBest answer
ST Technical Moderator
August 2, 2022

If the ULD API (STSW-IMG009) suites to you, please choose this one. It is simple, small, easy to use.

The full driver STSW-IMG007 is more complete but the simplest driver will do most of what you want.

If you don't need Linux nor Ultra Low Power, you can forget the two others.

Regards

Anne

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'

2 replies

Anne BIGOT
Anne BIGOTBest answer
ST Technical Moderator
August 2, 2022

If the ULD API (STSW-IMG009) suites to you, please choose this one. It is simple, small, easy to use.

The full driver STSW-IMG007 is more complete but the simplest driver will do most of what you want.

If you don't need Linux nor Ultra Low Power, you can forget the two others.

Regards

Anne

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'
DSai.1
DSai.1Author
Associate III
August 6, 2022

Dear Anne,

Thank you very much for your reply.

Based on your advise, we will port STSW-IMG007 to our RTOS for future

possible function extension.

best regards

Dai Sai