Skip to main content
DSai.1
Associate III
November 4, 2022
Question

about connection of pins in VL53L1X

Dear Sir,

We are going to make our own PCB after confirming the action with X-NUCLEO-53L1A1 module. We found the connection of pins 4, 6 12 in VL53L1X breakout board is different

with the Figure3 (VL53L1Xschematic) . In Figure 3, pins 4, 6 and 12 are connected to

main ground as same as described in Table2 (VL53L1X pin description). But in VL53L1X breakout board described in UM2359, pins 4 and 12 are connected to 1K resistors and pin 6 is not connected to any. We used schematic in Figure3 from datasheet. I wonder if there

is any problem for this schematic.

best regards

Sai Dai

,

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
November 14, 2022

The breakout board was designed before the chip was finished. So they left themselves plenty room to make changes. Use the schematic in the datasheet.

However if you were going to make any changes - may I suggest putting a decoupling cap very near each power pin? The schematic only shows one and tying the power pins together. 1 for each power pin would be better.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.