Skip to main content
HCabr.1
Associate
Mar 17, 2021 10:41 AM UTC
Question

Why am I not getting a DR fix?

Hello,

I'm currently using Teseo-VIC3DA Evaluation Board. I managed to get a 3D fix outdoors using DGPS. Afterwards, if I move indoors I get a "no fix" and I stop getting a position. Instead of this behaviour I would expect it would get into DR mode and compute the location based on the inertial unit and its sensors, which would be the correct behaviour, right? If so, do you have any suggestion to fix this behaviour?

I do not have an odometer connected to the module. Is there any procedure I should make or any configuration to be able to get a DR fix?

PS: When I record a trajectory, convert it to KML and open on Google Earth, I can see the “GNSS�? and “DR�? trajectories (they are always the same), but when I go indoors I lose both.

Best regards,

Hugo Cabrita

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Mar 17, 2021 12:08 PM UTC

    Does it need to attain sensor fusion before being able to report DR solutions?

    ​

    C​heck the expectations for fusion/calibration and meet those.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    HCabr.1
    HCabr.1Author
    Associate
    Mar 17, 2021 12:19 PM UTC

    Shouldn't it be able to compute a DR solution out-of-the-box? I currently do not have access to the DR panel as I do not have an activation key at the moment. Is that panel needed in order to configure DR?