Skip to main content
darla14
Associate III
Feb 2, 2021 7:38 AM UTC
Question

Where is the enable method/command in AN5203

Hello ,

I was checking this AN 5203 : https://www.stmicroelectronics.com.cn/resource/en/application_note/dm00528962-teseoliv3f--i2c-positioning-sensor--stmicroelectronics.pdf

on page 16 the main c code is written.

I wanted to know why we are not enabling the Teseo.I mean which method (if I am not able to find) is enabling the teseo or is it like it is default enabled when we power it ON?

I see the code directly inits the I2C and get the data over i2c?

One more question :

HAL_I2C_Master_Transmit(&hi2c1, 0x3A << 1, (uint8_t *)gpgll_msg, strlen(gpgll_msg), 2000)

>> what is 0x3A << 1 here ?

Is it the Teseo 7 Bit address?

one last question : Where Can I get the information on enabling and getting the similiar data (liek where can I find the list of all NMEA COmmands and thier corresponding commands like this : static const char *gpgll_msg = "$PSTMNMEAREQUEST,100000,0\n\r"; )

Many Thanks in advance !

D

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    Feb 2, 2021 7:47 AM UTC

    I2C here using 7-bit, STM32 expects these in the high order bits, so shifted there.​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    darla14
    darla14Author
    Associate III
    Feb 2, 2021 9:02 AM UTC

    Thanks @Community member​ 

    regarding enable what data should be sent to i2c?

    Is there a raw command set available? for enable,configuration and retrieving data?

    I am on arduino thats why asking in terms of raw data.

    Thanks,