Skip to main content
JOrta
Associate II
Jul 3, 2019 2:49 PM UTC
Question

What Options do I need to check on CubeMx if I only want the driver, the gnss library and the parser to do just basic stuff and start from scratch?

I am confused on what to add just to have the minimal function to read from the serial port the messages..0690X000009YNMiQAO.png

I am choosing this...

but i get duplicated pins.. not sure why

0690X000009YNNbQAO.png

0690X000009YNNlQAO.png

    This topic has been closed for replies.

    1 reply

    Andrea Palmieri
    ST Employee
    Jul 4, 2019 1:15 PM UTC

    ​Hi,

    to just enable the Driver and the Parser lib, you should check the "Board Extension" and the "Data Exchange" (Basic Interface, LibGNSS, LibNMEA) boxes.

    Kind regards