Skip to main content
yongjie989
Associate
Jan 10, 2024 1:45 AM UTC
Question

What are the differences in connecting with Teseo Suite and Terminal software?

Hello,

I am able to receive data normally when connecting USB with Teseo Suite, but when I connect using Terminal software, there is no data output at all. I am sure the baud rate is 460800. Is there a specific command I need to input for it to start outputting data?

I am using "Teseo EVB".

The connection with Teseo Suite is normal, and the data output is also normal:

yongjie989_0-1704850671029.png

However, when I use Terminal software to connect, there is no data output at all:
Is there a specific command I need to input for it to start outputting data?

yongjie989_1-1704850677737.png

Thank you.

 

 

This topic has been closed for replies.

1 reply

ST Employee
Jan 11, 2024 9:39 AM UTC

Hi

Teseo-Suite doesn't raise any command against Teseo-V to get it working.

Just because Teseo-V is powered it will works.

Please check on Terminal the baud rate and COM port and enable the Display has 'Hex' value.

 

Regards

 Francesco