Skip to main content
DAllo
Associate II
Jun 11, 2019 6:47 PM UTC
Question

TeseoIII carrier phase binary image

Please could someone point me in the direction of this binary? I'm wishing to acquire the raw carrier phase from our teseo-liv3f implementation.

    This topic has been closed for replies.

    6 replies

    Tesla DeLorean
    Guru
    Jun 11, 2019 7:26 PM UTC

    I was unable to get this and I tried quite hard.

    In talking to ST and others like myself doing RINEX and RTK stuff, it became apparent that the design is VERY noisy, the proximity of the QSPI Flash die to the baseband and RF downconverters is non-optimal. I tend to determine the effectiveness of a design implementation from the raw measurements.

    I also expressed interest in the Teseo V.

    I'm doing work with uBlox ZED-F9 L1/L2 GNSS receivers now.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    DAllo
    DAlloAuthor
    Associate II
    Jun 11, 2019 7:32 PM UTC

    Thanks, I obviously considered ZED-F9 but they're an order of magnitude more expensive. You are of course correct, I was hoping to perform RTK with the device. Has TeseoV seen daylight yet?

    ST Employee
    Jun 13, 2019 12:40 PM UTC

    Ciao

    Teseo-LIV3F doesn't support raw carrier phase.

    In ST we offer other Teseo 3 IC which supports raw carrier phase.

    Regards

    Francesco

    DAllo
    DAlloAuthor
    Associate II
    Jun 16, 2019 6:33 AM UTC

    Thanks, but I think that this binary is required for those IC to provide the carrier phase too. Before I respin a board design to use this other, could you please tell me where the binary is available from?

    DAllo
    DAlloAuthor
    Associate II
    Jun 16, 2019 6:34 AM UTC

    Thanks, but I think that this binary is required for those IC to provide the carrier phase too. Before I respin a board design to use this other, could you please tell me where the binary is available from?

    ST Employee
    Jun 17, 2019 8:11 AM UTC

    Hi

    On Teseo-LIV3F there is no firmware available to support Carrier phase.

    While in case of IC the firmware can be provided by local contact/FAE

    Regards

    Francesco