Skip to main content
Dror
Associate III
Dec 12, 2019 1:52 PM UTC
Question

TeseoIII Booting configuration

When boot configuration is set to boot over UART.

How can I use UART0 pins for flashing firmware instead of UART2?

The Xloader 2.2 only recognizes UART2 port for initial firmware flashing.

    This topic has been closed for replies.

    1 reply

    ST Employee
    Dec 13, 2019 9:30 AM UTC

    Hi Dror

    Booting from UART is running (simultaneously) on all the UARTs.

    When the core detects a byte from an UART.... it will go ahead with the whole protocol on the specific UART.

    At the end from Host side (or as pins configuration) nothing has to be modified,

    Hope this helps

    Regards

    Francesco