Skip to main content
Associate II
Aug 8, 2025 5:25 PM UTC
Question

Teseo-VIC3DA periodically outputs device version over UART – possible reset?

Hello,

I'm working with the Teseo-VIC3DA GNSS module on a custom board, and I’ve configured it to output both accelerometer and location data over UART.

However, I'm observing that periodically the device outputs a dump of its firmware version over UART. Similar to what is shown during boot. According to the datasheet, this kind of output usually occurs after a reset.

That said, I’ve been monitoring the GNSS fix, and it does not appear to be lost, even when this output occurs. I have monitored both the RESET and VDD lines and confirmed that the module is not being externally reset or power-cycled.

  • Is there any configuration setting or NMEA'0 command that could cause the Teseo-VIC3DA to periodically reprint the firmware version or behave as if it’s restarting?
  • Are there logs or debug outputs that can help distinguish between a soft reboot and a normal status message?

 

 

This topic has been closed for replies.

7 replies

ST Technical Moderator
Aug 12, 2025 2:27 PM UTC

Hi Rodrigo,

Could you please let me know what version of firmware, you are using ? 

Also, can you please read out of CDB registers for the following?

CDB-300 

CDB 230

Example how to get parameters

$PSTMGETPAR,1300

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
RGOrdeigAuthor
Associate II
Aug 13, 2025 2:26 PM UTC

This is the logs i get when resetting. I`m not sure what`s the firmware version you are referring to.
GNSSLIB_8.4.19.27.11_ARM
OS20LIB_4.4.0_ARM
GPSAPP_2.14.0.11_VIC3DA_ARM
BINIMG_4.6.18.11_VIC3DA_ARM
SWCFG_8406532d
STAGPSLIB_6.0.1_ARM
DRLIB_2.14.1_ARM
 STA8090_922bc043

I`ve sent $PSTMGETPAR,1300 and $PSTMGETPAR,1230.
This are the responses I`ve got:
$PSTMSETPAR,1300,1.000000e-01*4F
$PSTMGETPAR,1300*21
$PSTMSETPAR,1230,0x00000000*53
$PSTMGETPAR,1230*23

What are you looking for in this registers?

ST Technical Moderator
Aug 18, 2025 5:31 PM UTC

Hi Rodrgio,

I am running the following version, this is the latest version available on the web.

$PSTMVER,GNSSLIB_8.4.19.28.1_ARM*58
$PSTMVER,OS20LIB_4.4.0_ARM*40
$PSTMVER,GPSAPP_2.15.0.1_VIC3DA_ARM*00
$PSTMVER,BINIMG_4.6.19.1_VIC3DA_ARM*0F
$PSTMVER,SWCFG_8406532d*34
$PSTMVER,STAGPSLIB_6.0.1_ARM*5B
$PSTMVER,DRLIB_2.15.0_ARM*7E
$PSTMVER,STA8090_922bc043*60
$PSTMGETSWVER,255*17
$PSTMVER,GNSSLIB_8.4.19.28.1_ARM*58
$PSTMGETSWVER*09

 

Regarding seeing repeated PSTMVER message, after system boots, we get a PSTMVER message after the first 10 minutes. This is normal.

Can you please try with the latest version if possible?

Also I am assuming you have not changed any CDB settings from the default settings, have you ? 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.