Skip to main content
Associate
Sep 1, 2023 2:29 PM UTC
Question

TESEO-LIV4FTR

Hi there,

I recently got a sample TESEO-LIV4FTR chip.

I am used to rtk1010 from locosys, which seems similar in size. Not sure about the specifications.

 

Can this chip also acheive RTK cm level fix using a base or external ntrip server ?

 

Regards,

Adrian

This topic has been closed for replies.

4 replies

Issamos
Super User
Sep 1, 2023 2:55 PM UTC

Hello@xjust 

After a quick check , Find out that TESEO-LIV4FTR and rtk1010 are similar in almost everything . To understand more, I suggest you to take a look at the specifications of the  TESEO-LIV4FTR datasheet and compare them to those in the datasheet of the rtk1010 .

Hope this is helpful for you .

Best regards.

II

xjustAuthor
Associate
Sep 1, 2023 2:58 PM UTC

The datasheet I have doesnt specify much on LIV4F unfortunately. Hence the reason I asked here.

ST Employee
Sep 5, 2023 2:14 PM UTC

Hi

On Teseo-LIV4F you can not acheive RTK cm level accuracy.

you can try the Teseo-LIV4FM (which supports RTCMv3 protocol and carrier phase data) and run the RTK algorithm on an external host-micro.

 

ST Employee
Sep 28, 2023 2:29 PM UTC

Hi

> Can this chip also acheive RTK cm level fix using a base or external ntrip server ?

TeseoLIV4F (tape&reel Teseo-LIV4FTR) is a dualbands PVT only GNSS module.

It doesn't support raw measurement data.

As ST we introduced also Teseo-LIV4FM which provides raw measurement gnss data on RTCMv3 protocol.

With LIV4FM you can run an RTK algorithm on an external MCU using (as input data) the raw measurement the LIV4FM provudes.

Regards

 Francesco