Solved
Teseo-LIV4F position offset issue
- 4 replies
- 3131 views
Tested with FW ver.: 4.6.8.5.9 and 4.6.8.5.10
Data:
https://earth.google.com/earth/d/1mJeIeQjGAp2WDpIKkoNUQNGgshZ4bpLU?usp=sharing
I am working on a car tracking device and decided to use Teseo-liv4f, but during the tests I came to the following problem, as the GPS module shows the real position, it suddenly sends several coordinates 100 or 200 km from it, then returns back and starts showing the real position again. There are two examples in the link above from the uploaded data between points 84 and 87 and between points 759 and 763. The settings are standard for the firmware, only parameter 1303 has been changed from 1 to 0.2.