Skip to main content
Associate
Aug 21, 2023 6:12 PM UTC
Solved

Teseo-Liv4F pinout confusion

While researching the GNSS module for my project, I got somewhat confused about the power connection of the LIV4F module due to inconsistent information in the manuals. The general recommendation is to run at 1.8V for optimal power consumption, but my interface is running at 3.3V. In the evaluation board manual (UM3212), there's a 3.3V VCC_IO on pin 7 for communication and 1.8V VCC pin 8 for powering the module which would easily allow this set up. In the hardware manual (UM3004) for the module however, pin 7 is marked as reserved - which means there's no separate VCC_IO and I would need to level shift all the communication channels when running at 1.8V.

 

I was hoping you could clarify whether pin 7 is available as VCC_IO or not?

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 21, 2023 6:48 PM UTC

Welcome @Ikke, to the community!

Where did you find something about 1.8V, not including UM3212?

In general, the respective data sheets, not user manuals or application notes, are authoritative for the technical data and parameters. The data sheet of the LIV4F only contains the VCC and VBAT voltage ranges of 3.0...3.63V. Pin 7 was actually connected to VCC_IO in some predecessors of this module, but pin 7 is not to be used in the LIV4F.

The switch for VCC (3.3V/1.8V) visible in UM3212 is a remnant of a universal evaluation platform for Teseo-LIVxx, which is why the block diagram (fig. 19) also shows the module designation Teseo-LIV and not Teseo-LIV4F.

In summary, the LIV4F module must be operated with 3.0...3.63V.

Hope that answers your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 21, 2023 6:48 PM UTC

Welcome @Ikke, to the community!

Where did you find something about 1.8V, not including UM3212?

In general, the respective data sheets, not user manuals or application notes, are authoritative for the technical data and parameters. The data sheet of the LIV4F only contains the VCC and VBAT voltage ranges of 3.0...3.63V. Pin 7 was actually connected to VCC_IO in some predecessors of this module, but pin 7 is not to be used in the LIV4F.

The switch for VCC (3.3V/1.8V) visible in UM3212 is a remnant of a universal evaluation platform for Teseo-LIVxx, which is why the block diagram (fig. 19) also shows the module designation Teseo-LIV and not Teseo-LIV4F.

In summary, the LIV4F module must be operated with 3.0...3.63V.

Hope that answers your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
IkkeAuthor
Associate
Aug 21, 2023 8:40 PM UTC

Dear Peter,

Thank you, that's what I needed to know!

As for the 1.8v, there's also the reference on page 4 of the hardware manual, which says "To optimize battery current consumption, it is possible to use a SMPS at 1.8 V to supply VCC."

Peter BENSCH
ST Technical Moderator
Aug 22, 2023 7:33 AM UTC

Once again: relevant for the parameters of the respective component is always and exclusively its data sheet.

But let's break it down: the UM3004, rev 2 is obviously older (2022-11) than the data sheet, rev 4 (2023-07) (later readers please pay attention: could change in the future). It is very likely that at some point during the development of the LIV4F, it was planned to specify it from 1.8V as well. Then the UM3004 was written, where the talk is about this voltage. But later it turned out that the module cannot be guaranteed to work 100% from 1.8V, so it was specified for 3.3V only - and unfortunately they forgot to take the relevant section out of the UM3004. The first sentence of this post applies again here at the latest.

But one more remark (attention, subjunctive!): even if the 1.8V had been specified, the same voltage would have applied to the IOs. So either level shifters would have been necessary to connect a 3.3V MCU, or the MCU would also have had to run on 1.8V. But as I said, this is all hypothetical, since the specification is 3.3V.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Jul 23, 2025 12:15 PM UTC

Hello,

I have a design that is working with 3.3V from other vendor.

Pin 7 is used as VCC_IO and it 3.3V.

The question is, can I replace and put the LIV4F instead?

What will happen if pin 7 will get 3.3V (instead of being not connected)?

Any chance of harm or malfunction?

I don't expect logic issue since I'm working with 3.3V (and no conflict with past pin configuration as VCC_IO)

 

tizdipietro
Associate III
Jun 9, 2026 4:07 PM UTC

Hi ​@Peter BENSCH 

I stepped across this while I'm trying to integrate the Teseo LIV4F as a replacement to the Teseo LIV3FL in the current pcb design. As previously noticed, there is still the mention of the 1.8V in UM3004 in section 2.0 and 2.3 (current version on your website). Can you please confirm that the Teseo LIV4F only accepts 3.3V?

 

Additionally, the Fig.2 of UM3004 is suggesting 10uF decoupling on VCC, this seems very strange to me. I would have expected something in the range of 0.1uF honestly. is there any reason for this, or is this a mistake as well (because then the x-nucleo-LIV4A1 uses 100pF and 0.1uF). Which of the both is the correct implementation?

And since I’m looking at the X-NUCLEO-LIV4A1 Schematic: it seem like the third page is the copy of the first one, but the entire RF section is missing instead. Would be grate if you could share the corrected version.

Thanks

Peter BENSCH
ST Technical Moderator
Jun 9, 2026 7:51 PM UTC
  1. The UM3004 was last updated in rev. 4 on 29/11/2023, whereas the datasheet for the TESEO-LIV4F was updated on 30/05/2024 (rev. 6) and then on 2/3/2026 (rev. 7). The more recent document should actually contain the more relevant data, do you agree?
    But as mentioned previously, when it comes to electrical and other parameters, the datasheet is fundamentally decisive - always. In that respect, it is self-evident that only the specified range is authorised as VCC, namely 3.0...3.63V.
  2. The question about the buffer capacitor is very interesting. However, here too it can be assumed that the UM3004 a) is already somewhat older and b) that a certain safety margin was built into the design; the colleagues there were probably still assuming a minimum VCC of 1.8V.
    It would not, however, do any harm to use 470nF or 1µF instead of 100nF; it is only important to connect it to VCC as closely and with as low resistance as possible.
  3. Well spotted!
    Perhaps ​@GalaxyQuest has access to the correct schematics, which, by the way, are also incorrectly included in DB5161 and in UM3296.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.