Skip to main content
RVerv.1
Visitor II
Jun 21, 2020 11:54 PM UTC
Question

Teseo LIV3x

Hello,

I’m looking into buying a Teseo LIV3x module (one of both). What I saw in the datasheets is that they accept RTCM messages, is that true? Does this mean that if I give the module these messages, it will output corrected nmea sentences?

I saw that there is a binary which you can flash so that it outputs raw measurement data. So theoretically I should be able to use it with RTKlib?

I was searching for answers on these questions, but can’t find much info on this.

I dont need to make myself a RTK base station, because in my country (Belgium), there is a free service (FLEPOS), which we can use to get NTRIP.

kind regards

Raf

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Jun 22, 2020 1:34 AM UTC

    >>I saw that there is a binary which you can flash so that it outputs raw measurement data. So theoretically I should be able to use it with RTKlib?

    My understanding was that the measurements were very noisy

    The RTCM3 would only support DGPS/SBAS type pseudo-range correction as I understand it.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ST Employee
    Jun 29, 2020 8:51 AM UTC

    Hi

    >  What I saw in the datasheets is that they accept RTCM messages, is that true

    Yes. LIV3F suspport RTCM v2.3

    > I saw that there is a binary which you can flash so that it outputs raw measurement data. So theoretically I should be able to use it with RTKlib?

    No. You can't.

    ST provides pre-builded binary. You can not flash a generic binary. in detail there is no LIV3F binary which provides raw measurement data.

    Hope this helps

    Regards

    Francesco