Skip to main content
AMoro.16
Associate
Jul 23, 2021 6:34 PM UTC
Question

TESEO LIV3R no coordinates

Hello. I've developed the board based on TESEO LIV3R module. I have successfully developed and debug code on X-NUCLEO GNSS1A1 and it get position from the GNSS receiver perfectly. When I run the same code on my board, I receive NMEA messages with 0. No position, no speed, no time, 99 satellites..

I attached my schematic. I use chip antenna 1575AT43A0040E. Can anyone help, what is wrong?

    This topic has been closed for replies.

    4 replies

    DZhou.1
    Associate
    Jul 23, 2021 6:41 PM UTC
    Check out antenna connection for the GPS first. Or try it outside the building.
    David
    AMoro.16
    AMoro.16Author
    Associate
    Jul 23, 2021 6:50 PM UTC

    Thank you for the answer. Outside the building situation is the same. What do you mean under "Check out antenna connection for the GPS first"?

    Tesla DeLorean
    Guru
    Jul 23, 2021 6:49 PM UTC

    Not going to fish part# out of bitmaps.

    Check that your RF amplifier is powered and enabled, check logic state on pins.

    You could try injecting RF at various points from a known working GNSS antenna source you've got powered via a splitter.

    You could check circuit/antenna tuning with a network analyzer.

    Be outside to get the best signals, avoid the human body in proximity to the chip antenna.

    Perhaps consult with an ST GNSS FAE

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    GQuin.2
    Visitor II
    Mar 24, 2023 10:17 AM UTC

    Did you manage to solve it? I'm about to use this GNSS but I'm not sure if it will work with passive antenna