Skip to main content
Gero
Associate II
Jun 11, 2019 11:31 AM UTC
Question

TESEO III accuracy

Hi,

Doing randoms tests on the TESEO III accuracy, I've found an horizontal accuracy of 14m for 95% of the locations with extremes of 23m. Does ST have more informations about the TESEO III accuracy ? Are there tests that have been published ?

Thanks

Regards

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    Jun 11, 2019 12:09 PM UTC

    I'm sure they have published CEP specs.

    Your results do seem particularly awful, but I think that's on you and your antenna or RF side. Does not seem consistent with a properly executed test. When peopl​e generate spec numbers it is usually with very expensive and very well placed antennas to provide optimal results.

    ​

    I've posted plots to this GNSS subforum.​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    Jun 11, 2019 12:25 PM UTC

    https://community.st.com/s/feed/0D50X00009ZEutBSAT

    CEP99 well inside 5m, and the bulk of the hits well inside 2.5m

    Make sure you don't have airflow over the IC or TCXO

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Gero
    GeroAuthor
    Associate II
    Jun 11, 2019 1:08 PM UTC

    Thanks !

    Are you using SBAS ?

    ST Employee
    Jun 13, 2019 12:51 PM UTC

    Ciao

    Teseo3 in the default configuration guarantees:

    • 1.5m CEP50 (this is public result in the DS)

    and we are close to

    • 2m CEP90

    I think there something strange in your platform.

    SBAS is On by default in ST firmware.

    Regards

    Francesco