Skip to main content
Associate II
Nov 20, 2025 4:11 AM UTC
Question

TEOSEO VIC3DA can not get message PSTMDRCAL

Dear St's engineers,

I am encountering an issue with the GNSS TESEO VIC3DA module regarding the inability to enable the PSTMDRCAL message output. I have tried the command $PSTMSETPAR,1228,0x800000,1*4F (as described in the CDB table 228, which is used to enable three messages: PSTMDRGPS, PSTMDRCAL, PSTMDRSINT), but as a result, only PSTMDRGPS is being output.

1 reply

ST Technical Moderator
Feb 3, 2026 7:36 PM UTC

Hi,

If you are not using wheel tick input or sending speed information over UART, then Teseo VIC3DA is considered in DRUM (Dead Reckoning Unplugged Mode). 

The $PSTMDRCAL is only sent when when wheel-tick or speed over UART is present. This is considered DRAW mode. (Dead Reckoning Automotive way)

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.