Skip to main content
Associate II
Nov 17, 2024 7:25 AM UTC
Question

Taseo-LIV4F Firmware Upgrade for NavIC

While upgrading Taseo Firmware for NavIC through UART interface to PC, I got the following error message:

Upgrade command error
Please check software baud rate or select recovery mode


My setting are:
Loader baud rate: 115200
Software baud rate 115200

Jumper settings

J6:2-3 (FW-UPG)

J7: 2-3(FW-UPG)

J11: NC

Request to confirm the correct baud rates or how to upgrade the firmware.

This topic has been closed for replies.

2 replies

Visitor II
Nov 17, 2024 8:02 AM UTC

Check if both the loader baud rate and the software baud rate match, as they do in your settings (115200 in this case).

Associate II
Nov 17, 2024 5:18 PM UTC

Thanks for your reply.

The problem is fixed now. Earlier, I was using 40 pin connector Rx and Tx pins which then I changed to J10 Rx and Tx.