Skip to main content
Visitor II
Mar 20, 2025 10:42 AM UTC
Question

synchronizing multiple GNSS receivers (Teseo v)

Hi.

I want to use two GNSS receiver ICs from the Teseo v family (either STA8100 or STA8135).

It is important in my application that the 3-bit ADC sampling of both receivers will be synchronized.

The IC has a TCXO input which obviously is used as the reference for the down-conversion LO PLL circuit.

Is this TCXO input used as the source for the ADC clock as well? or is the clock sourced from an internal oscillator?

 

Thanks,

Yonatan

This topic has been closed for replies.