Skip to main content
sougata
Associate II
Oct 29, 2021 9:06 AM UTC
Question

STAGPS Testing fails to download the Rinex file

Hi,

I am trying to test the COLD START behaviour of the X-NUCLEO-XGNSS1A1 and when trying to start the Autonomous mode I get the following response:

Running Autonomous AGPS task

Rinex files directory is D:\RINEX

Start downloading file ftp://cddis.gsfc.nasa.gov/pub/gps/data/campaign/mgex/daily/rinex3/2021/brdm/brdm3010.21p.Z

Operation cancelled

System.Net.WebException: The request was aborted: The request was canceled.

  at System.Net.FtpWebRequest.EndGetResponse(IAsyncResult asyncResult)

  at System.Net.WebClient.GetWebResponse(WebRequest request, IAsyncResult result)

  at System.Net.WebClient.DownloadBitsResponseCallback(IAsyncResult result)

--- End of stack trace from previous location where exception was thrown ---

  at System.Runtime.CompilerServices.TaskAwaiter.ThrowForNonSuccess(Task task)

  at System.Runtime.CompilerServices.TaskAwaiter.HandleNonSuccessAndDebuggerNotification(Task task)

  at STGps.TWebReq.<StartTaskDownloadFileAsync>d__8.MoveNext()

Task aborted!

I cannot download the file manually too. Please help.

0693W00000GVseGQAT.jpg

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Oct 29, 2021 10:00 AM UTC

    Check if any files exist in that directory or tree. Data location may have been moved or changed due to abuse by bots. Check for documentation or change notifications from the data provider.​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    sougata
    sougataAuthor
    Associate II
    Oct 29, 2021 10:02 AM UTC

    Hi,

    Thanks for the reply

    I tried to explore the ftp: but anonymous login is not supported. And for the local Directory to save the RINEX, I can confirm that it is empty