Skip to main content
rnieto
Visitor II
Oct 27, 2022 7:28 AM UTC
Question

STA8135GA configuration with EVBT5MCM

Deal all,

I borrowed an evaluation board EVBT5MCM to a colleague in order to evaluate the 1 PPS performance over some configurations. I downloaded the Teseo suite software and I saw NMEA messages related to the configuration such as $PTMXXX like. I achieved to change the 1 PPS configuration but I tried the same with the used constellations ($PSTMCFGCONST and $PSTMSETCONSTMASK) with no success and even not possible to get any reply message. I also tried to disable NMEA if that helps to send commands but I lost the NMEA interface. I have checked the offical documentation but I did not find any solution. Please, could anyone to help me in this setup? I checked also that an updated of the firmware could add a particular documentation however I don't have available firmware binaries.

Thank you in advance,

Cheers

Raul Nieto

    This topic has been closed for replies.

    1 reply

    ST Employee
    Sep 28, 2023 2:49 PM UTC

    Hi

    > $PSTMCFGCONST and $PSTMSETCONSTMASK

    These commands are related to Teseo3 IC and modules.

     EVBT5MCM embeds the STA8135 IC (Teseo5) which uses a differet configuration block layout and the 'STMCFG' commands are not supported.

    You can have a look on 'AN_Firmware_Configuration.pdf' document in the firmware release folder to see know configure the Teseo5 solution.

    Regards

     Francesco