Skip to main content
Gero
Associate II
Mar 28, 2019 8:28 AM UTC
Question

[SOLVED] [CLOE BOARD] What is the minimal code needed to have an UART communication ?

Hi,

I'm using a Sequans CLOE board for one of my project. All the development code provided with the board are hard to understand. Is there a simple code juste to initialise the uart communication and to start using the GNSS API ?

The CLOE board soft runs on a TESEO III on the board.

As all the codes are comming from ST, Sequans can't answer these questions.

Edit: There are some 2MB version of the TESEO III instead of the classic 4MB present on the CLOE. Try to remove the configuration number 250->15 in fwcfg.txt

    This topic has been closed for replies.

    3 replies

    ST Employee
    Mar 28, 2019 12:55 PM UTC

    Hi

    On the CLOE board you should ask to Sequans (www.sequans.com) as they are the platform's owner.

    > As all the codes are comming from ST, Sequans can't answer these questions.

    Sequans is in charge of customer support.

    Regards

    Francesco

    Gero
    GeroAuthor
    Associate II
    Mar 28, 2019 1:17 PM UTC

    Thank you for your answer. It's very annoying to work on this platform. Sequans and ST are always sending me back to one another.

    In fact, the codes are signed by ST, the chip is a ST and the documentations are made by ST. So I think the best way to get an answer isn't to ask Sequans, and they wouldn't answer anyway.

    So please can you reconsider my question ?

    MBoti
    Visitor II
    Mar 29, 2019 3:50 PM UTC

    Dear Gero,

    This is Manuel from Sequans Communications

    I am very sorry for your experience. Note that CLOE is not a mass market platform so we usually do not do support via public forum. Please contact me at mbotija (at) sequans (dot) com and I will provide you the necessary support.

    Best,

    Manuel