Skip to main content
Dror
Associate III
Dec 12, 2019 8:44 AM UTC
Question

NMEA 230400 baud rate with Teseo-Suite Pro 6.1.3.0

Hi,

I am using the suite with a TeseoIII set to output at 230400 baud rate.

When in this rate the suite does not auto-detect it and does not connect automatically as it does in 115200.

When configured manually to this rate, it can communicate and show the signal level, but in this rate it cannot open the skyview, the Firmware wizards cannot start and the firmware configuration panel cannot start.

Do you have a newer tool version that is capable to resolve the above?

Thanks.

    This topic has been closed for replies.

    9 replies

    ST Employee
    Dec 16, 2019 2:12 PM UTC

    Hi Dror

    Sorry for the delay.

    TS is able to detect a device but only with predefined baud rate.

    The (on startup) baudrate can be configured in:

    Menu->File->Prefereces->'Detect devices at start-up' radio-buttons

    Let me know if this fixes the issue.

    Regards

    Francesco

    Dror
    DrorAuthor
    Associate III
    Dec 16, 2019 3:30 PM UTC

    Hi,

    I can see the radio buttons but the only options there are 115200 or 9600. No other baud rate options are available.

    Also, please note my other comments. If manually configured to 230400 rate, the skyview button has no effect and the "FW configuration panel" cannot be activated.

    Please check.

    Thanks.

    ST Employee
    Dec 17, 2019 9:44 AM UTC

    Hi Dror

    I just did a test with Teseo-Suite 6.3.3 @ 230400 and it seems working for me.

    I just sent the program to you using https://mft-eu.st.com/.

    Let me know

    Regards

    Francesco

    ST Employee
    Dec 17, 2019 9:44 AM UTC

    Hi Dror

    You should reveice an email to download the file

    Regards

    Francesco