Skip to main content
Iyaku
Associate II
Oct 30, 2019 2:54 PM UTC
Question

My TESEO-LIV3F has stopped connecting to the Teseo-Suite! How can I restore factory settings?

..

    This topic has been closed for replies.

    16 replies

    ST Employee
    Oct 30, 2019 3:05 PM UTC

    Hi

    Did you change anything in the firmware configuration?

    Which tool are you using? EVB-LIV3F or X-Nucleo-GNSS?

    Thanks

    Regards

    Francesco

    Iyaku
    IyakuAuthor
    Associate II
    Oct 30, 2019 3:20 PM UTC

    Yes, I tried to configure the firmware. But the process freezes and Teseo no longer communicates with the PC.

    No I do not use VB-LIV3F or X-Nucleo-GNSS.

    I have a Teseo module soldered to the board.

    ST Employee
    Oct 30, 2019 3:26 PM UTC

    From your MCU-host you should perform a firmware-update where the configuration is removed.

    You can take the firmware @ https://www.st.com/content/st_com/en/products/embedded-software/automotive-infotainment-and-telematics-software/teseo-liv3fsw.html

    Take care that to perform firmware-update your MCU has to driver the Teseo-LIV3F.nReset pin.

    Just a question: what were you configuring? may be it's just a baud-rate issue?

    Did you see PPS blinking? May you can communicate with I2C port.

    Regards

    Francesco

    Iyaku
    IyakuAuthor
    Associate II
    Oct 30, 2019 8:37 PM UTC

    But can I complete firmware-update where the configuration is removed from the PC and terminal program or using any other program?

    ST Employee
    Oct 31, 2019 8:13 AM UTC

    Hi

    Firmware update is always possible because internally it doesnt' care on the configuration.

    On the PC:

    • you have to use the firmware update tool (in the Teseo-Suite);
    • in the firmware update tool you have to enable:
      • Recovery mode
      • Erase NVM
      • Baud 115200

    On the board:

    • connect the UART
    • Push "Start" button in the firmware-update tool
    • Trigger the module reset (this is mandatory)

    On Module reset the firmware update will start.

    Hope this helps

    Regards

    Francesco

    Iyaku
    IyakuAuthor
    Associate II
    Nov 4, 2019 7:39 AM UTC

    Hi

    So that's the point, Teseo-Suite throws an error when you press the STA808x / 9x FW Upgrade button in the Tools menu?

    0690X00000ArcnlQAB.jpg0690X00000ArcngQAB.jpg

    Iyaku
    IyakuAuthor
    Associate II
    Oct 30, 2019 8:40 PM UTC

    speed did not change exactly

    Worked only on UART, PPS is not possible to control.