Skip to main content
Associate
Apr 30, 2024 11:22 AM UTC
Solved

LIV4F actual VBAT range

What is the actual backup input supply voltage range for Teseo LIV4F receivers? Datasheet says that it is 3-3.63V which is really high and doesn't make sense to add any Lithium battery as a backup supply because it will very quickly drop below 3V at the beginning of operation (CR2032/CR1220). But X-NUCLEO-LIV4A1 (https://www.st.com/resource/en/data_brief/x-nucleo-liv4a1.pdf) has a place for CR2032 battery socket and even diode D2 in series on which will be some extra voltage drop. So the question is it a mistake in board design or the actual minimum VBAT voltage is less than it's written in the datasheet? In the second case, it's a drawback of these receivers, at least for my use-case.

This topic has been closed for replies.
GalaxyQuestBest answer
ST Technical Moderator
May 3, 2024 3:34 PM UTC

LIV4F VBAT can operate down to 2.1V.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

4 replies

ST Technical Moderator
May 1, 2024 5:55 PM UTC

I believe there is a margin that will allow for VBAT to dip below 3V.

Please give me a day or two to confirm this.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
VaneAuthor
Associate
May 2, 2024 7:40 AM UTC

Thanks! It would be nice to check. If it can operate at 2.5V, it will be sufficient for use with lithium batteries.

GalaxyQuestBest answer
ST Technical Moderator
May 3, 2024 3:34 PM UTC

LIV4F VBAT can operate down to 2.1V.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
VaneAuthor
Associate
May 6, 2024 8:00 AM UTC

Thank you! That's very nice.