Skip to main content
Visitor II
Jun 12, 2025 10:13 PM UTC
Question

LIV4F

Is a document available that defines all the configuration data blocks for the LIV4F?  We are specifically looking for the contents of configuration data block 263, which seems to configure the I2C interface.

This topic has been closed for replies.

1 reply

ST Technical Moderator
Jun 18, 2025 1:43 PM UTC

Hi,

You can enable the I2C interface by

 

$PSTMSETPAR,1263,0x1,1 //enable I2C 
$PSTMSAVEPAR //save and reset
$PSTMSRR //reset for settings to take effect

$PSTMSETPAR,1263,0x1,2 //disable I2C with bit mask 2 
$PSTMSAVEPAR //save and reset
$PSTMSRR //reset for settings to take effect

 

I2C speed by default is set to STANDARD.

Bit 16-23
0..2
0 = Speed mode STANDARD
1 = Speed mode FAST
2 = Speed mode HS

Default device address of LIV4F is 0x3A.

I would not change bit-24 to bit-31 as this deals with pin assignment and is not applicable for module settings.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.