Skip to main content
PTsen
Associate III
Jan 21, 2019 7:09 PM UTC
Solved

Issues on Setting Parameter

Hi, I have tons of question about the command $PSTMSETPAR and some related command:

​

First of all, I would like to change the NMEA Baudrate to 38400, as the software manual said, I should transfer

​

"$PSTMSETPAR,1102,0x8"

"$PSTMSAVEPAR"

​

and NMEA gives me the result (no comma due to the way I'm processing the string):

​

$PSTMSETPAROK 1102*31

$PSTMSETPAR 1102 8

​

as the manual says, I should reset the system, so I've enter the command "$PSTMRR", and it returns "$GPTXT DEFAULT LIV CONFIGURATION*2B". But when I change my Baudrate from 9600 to 38400, I got scribbled message, only when I change back to 9600 will the message be shown properly. However, after I unpowered my stm32 and power it again, I ""sometime"" find it changes its Baudrate to 38400, vice versa. So here are my questions:

​

  1. How to reset X-NULCEO-GNSS1A1: As I dig into the example code from cubeMS, I found that reset is done by setting low on the reset pin, wait for a while, then setting it to high, then wait for a while, but doing so doesn't make any change to the setting. So I'm not sure how the resetting is done.
  2. Should I send the second command after the previous command got the return message? E.g. I should wait "$PSTMSETPAROK 1102*3" after sending the command "$PSTMSETPAR,1102,0x8" , then send the new command, or I can send "$PSTMSETPAR,1102,0x8" followed by "$PSTMSAVEPAR" immediately?

​

Next, I would like TESEO LIV3F to send to me only some certain message, say, $GPGGA, to do so, I need to use the command $PSTMCFGMSGL, and here is my next group of questions:

​

  1. From "Application note - AN5203 - Teseo-LIV3F - I2C Positioning Sensor", I found an example of setting the config is done as follow:

$PSTMCFGMSGL,3,1,0,0
$PSTMSETPAR,1227,1,2 
$PSTMSAVEPAR

​

I can't understand, from the software manual of Teseo-LIV3F, the syntax of $PSTMCFGMSGL is <listid>,<rate>,

<list_l>,<list_h>*<checksum><cr><lf>, where listid can only be 0 or 1, I don't even know what listid 1 is since I can't

find the CBD_ID 210 and 229 relevant to msg list in the user manual, not to mention the value 3 in the example

above, also, I don't know what does "rate" here mean.

​ 2. After reconfigure the message list by the command "$PSTMCFGMSGL,0,1,0,0" and "$PSTMSAVEPAR", nothing

changed, I'm expecting this since the Baudrate doesn't change immediately, as well. When I request the

message via command $PSTMNMEAREQUEST,100000,0 (GPGLL), I didn't get what I expected, instead, I get this

​

0690X000006DBGRQA4.jpg

​Which is totally different from the application note, and I don't know what to do, the manual is rather confusing to me.

Any advice would be great, since I'm literally having hard time getting this module to work. Thank you.

    This topic has been closed for replies.
    ST Employee
    Jan 25, 2019 9:16 AM UTC

    > we should append checksum and cr, lf at the end of the string

    Yes. correct.

    > which has the wrong checksum, what is happening?

    Really strange. I tryed all the commads and they work on my side.

    Could you check your code?

    Do you want share?

    Just a note (sorry I forgot to say) but the whole C-Driver for Teseo-LIV3F is already online @

    https://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-gnss1.html

    in the package you will find binary for STM32 and all the C-Code. May be it could help your development.

    Regards

    Franceco

    8 replies

    ST Employee
    Jan 22, 2019 8:11 AM UTC

    Hi

    To change NMEA baudrate you can use the following script:

    ====

    $PSTMCFGPORT,0,0,2,new_baud_value

    $PSTMSAVEPAR

    $PSTMSRR

    ====

    1. How to reset X-NULCEO-GNSS1A1

    You can perform a software reset using the commands "$PSTMSRR" or an hardware reset toggling the pins Teseo-LIV3F.nReset (pins Connector-9_pin-8 on the X-Nucleo-GNSS1A1)

    > I would like TESEO LIV3F to send to me only some certain message

    I2C anc UART ports have separated message-list.

    To change the UART-message-list you can use the following scripts:

    ==================

    $PSTMCFGMSGL,0,1,<list_low>,<list_high>

    $PSTMSAVEPAR

    $PSTMSRR

    ==================

    Let me know if this helps.

    Regards

    Francesco

    PTsen
    PTsenAuthor
    Associate III
    Jan 24, 2019 8:27 AM UTC

    Hi, thanks for your response

    First of all

    ===

    $PSTMCFGPORT,0,0,2,0x5

    $PSTMSAVEPAR

    $PSTMSRR

    ===

    What I expected: As soon as I do the software reset, the baudrate of NMEA should be the new one.

    What turns out to be: The baudrate of NMEA doesn't change since changing the USART baudrate to the new one result in scribbled message, but is normal when change to original baudrate

    Additional question: what does '2' mean here? According to the manual, I see the first param is portnumb (UART GPIO ID), what ID?

    Next,

    ==================

    $PSTMCFGMSGL,0,1,0,0

    $PSTMSAVEPAR

    $PSTMSRR

    ==================

    What I expected: As soon as the software reset, I should receive nothing

    What turns out to be: The message keeps printing as if nothing happened.

    ST Employee
    Jan 24, 2019 9:04 AM UTC

    Hi

    > $PSTMCFGPORT,0,0,2,0x5

    It should be:

    $PSTMCFGPORT,0,0,2,115200

    or

    $PSTMCFGPORT,0,0,2,9600

    to restore the default setting

    >  what does '2' mean here?

    Teseo-III has several UART port (The UART-2 is the one available on the module).

    > What I expected: As soon as the software reset, I should receive nothing

    Just tested and working on my side.

    The periodic messages are no more sent from the module.

    Could you check?

    Thanks

    Regards

    Francesco