Skip to main content
DTali
Associate II
Jun 11, 2019 1:51 PM UTC
Question

incorrect phase measurements with TESEO LIV3F

I have measured phase difference and get wrong data.

Help me please to find solution.

0690X000008iU3EQAU.png

A1 - antenna 1

A2 - antenna 2

S - satellite

Sat pos 1 - satellite position in T1

Sat pos 2 - satellite position in T2

В - A1-A2 lenght (5m)

Cos(α1)= λ*(Ф2-Ф1)/(2*π*B)=λ*(φ12-φ11+k)/(2*π*B)

φ11, φ12 - pseudophase, read from receiver

k - number of ambiguity cycles

Cos(α2)=λ*(φ22-φ21+k)/(2*π*B)

Cos(α2)-Cos(α1)=λ*((φ22-φ21)-(φ12-φ11))/(2*π*B)

Cos(α2)-Cos(α1)=λ*Δφ/(2*π*B)

Δφ=2*π*B*(Cos(α2)-Cos(α1))/λ

A1 coordinates in WGS84:

x=2352338.526

y=2718871.727

z=5250711.535

A2:

x=2352337.383

y=2718876.244

z=5250709.721

T1=133200 (13h 32m 00s UTC)

T2=133201

SatPos1:

xj1=-16213258.59

yj1=7225892.91

zj1=19698260.91

SatPos2:

xj2=-16215421.53

yj2=7224579.41

zj2=19696990.78

Cos(α1)=0.12834301654361024

Cos(α2)=0.1283298031315633

Phase difference calculated from coordinates:

Δφ=2*π*B*(Cos(α2)-Cos(α1))/λ=-0.002181426087639554

Phase Difference Received from Receiver (PSTMTS message):

Δφ=(φ22-φ21)-(φ12-φ11)=(-51388.13+51106.71)-(-51387.36+51106.91)=-0.97

    This topic has been closed for replies.