Skip to main content
AAl S.1
Associate III
Jun 11, 2020 11:59 AM UTC
Solved

Hi, I want to connect Teseo-Liv3R to an active antenna. I have seen in the Data sheet section number 6.2 how to connect it. My questions:

1- What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?

2- I have seen in the   in section 7 general schematic. Is it for passive antenna only?

Thanks

best regards

    This topic has been closed for replies.
    ST Employee
    Jun 29, 2020 8:44 AM UTC

    > What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?

    fig.10 and Fig11 are similar. In the second case (fig.11) the switch works also as current limiter

    There is a type in the image S22943 stands for TPS22943.

    >2- I have seen in the   in section 7 general schematic. Is it for passive antenna only?

    Yes.

    Regards

    Francesco

    1 reply

    ST Employee
    Jun 29, 2020 8:44 AM UTC

    > What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?

    fig.10 and Fig11 are similar. In the second case (fig.11) the switch works also as current limiter

    There is a type in the image S22943 stands for TPS22943.

    >2- I have seen in the   in section 7 general schematic. Is it for passive antenna only?

    Yes.

    Regards

    Francesco