Skip to main content
PRona.1
Associate II
Jan 15, 2020 8:50 AM UTC
Question

Having problems connecting my STEVAL-STRKT01 with Teseo Suite Pro 5.2 Is there a step by step guide of what to do once the eval board is un boxed?

..

    This topic has been closed for replies.

    8 replies

    ST Employee
    Jan 15, 2020 9:03 AM UTC

    Hi PRone

    sorry but how are you connecting the board with the PC?

    the USB connector on the board is NOT connected to the module.

    You can find the Rx/Tx signal of the module on CN503 connector .... but they are pure UART signals... and you should use an UART2USB to connect the signal to the PC.

    Thanks

    Ciao

    Francesco

    PRona.1
    PRona.1Author
    Associate II
    Jan 15, 2020 10:47 AM UTC

    Hi Francesco,

    Thanks for the quick reply.

    I was connecting to the PC using the USB-C cable provided in the kit and following the instructions in UM2541.

    When I connect to Tera Term using the USB only at a Baud rate: 115200 I get data seen in the image attached.


    _legacyfs_online_stmicro_images_0690X00000Bw14x.png

    When I connect to Tera Term over UART I see the data in a different format in the second image attached.
    _legacyfs_online_stmicro_images_0690X00000Bw16j.png

    So based on this it is not getting any sats therefore co-ordinates are always 0,0,100

    There is a sending joined request in the image below do I need to complete some additional tasks to enable geo-location


    _legacyfs_online_stmicro_images_0690X00000Bw18u.png

    I just want to demonstrate the module finding sats and acquiring its location for now as I am hoping to use the Teseo LIV3F in a larger design we are working on.

    Regards,

    *****

    ST Employee
    Jan 15, 2020 11:02 AM UTC

    Ciao

    Take care you have to use the evaluation board in open sky condition.

    Is it the case?

    Regards

    Francesco

    PRona.1
    PRona.1Author
    Associate II
    Jan 15, 2020 11:16 AM UTC

    Hi Francesco,

    Sorry for my ignorance new to gps. when you say open sky you mean outside right?

    So the reason I don't see sats and can not connect in Teseo-Suite Pro is because I need to be outside or atleast in view of the sky?

    Regards,

    *****

    PRona.1
    PRona.1Author
    Associate II
    Jan 15, 2020 3:18 PM UTC

    Hi Francesco,

    Thanks so much for all the information it has really helped in my evaluation of the Teseo-LIV3F and I will definitely be using it in the upcoming project.

    I know the STEVAL-STRKT01 is also a LoRa Tracker and I can't see the DevEUI in Tera Term. Is there a command to read it back.

    GNAST.1
    Visitor II
    Jan 16, 2020 10:17 AM UTC

    ​Hi Prona.1,

    as you have had the opportunity to experiment, the STEVAL-STRKT01 allows exchanging data with an USB device.

    The STEVAL-STRKT01 also allows you to send commands. The list of supported commands is included in the UM2487 (Table 2) and UM2541 (Table 1).

    Among these, the ?devicejoinparam command  gets all the LoRa keys, including the DevEUI. Furthermore, the DevEUI parameter together with joinEUI, application key and network key, can be set by using the following commands sequence:

    !deviceeuixxxxxxxxxxxxxxxx

    !joineuixxxxxxxxxxxxxxxx

    !appkeyxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx

    !ntwkkeyxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx

    x is a nibble.  So it means you have replace all the x according to the provisioning keys that you want to set.

    After the four commands, restart the board with the !sysreset command.

    Remember that all ASCII commands must end with the <CR> <LF> characters (where <CR> is the 0x0D carriage return byte and <LF> is the 0x0A line feed byte).

    Regards,

    Giuseppe