Skip to main content
FreakStudio
Visitor
July 23, 2026
Question

Embedded System Beginner's Guide: Distinguish Chips from Development Boards in 5 Minutes, Starting with Raspberry Pi Pico

  • July 23, 2026
  • 0 replies
  • 4 views

1. Introduction to Raspberry Pi Pico

The Raspberry Pi Pico is a low-cost, high-performance microcontroller development board officially designed by Raspberry Pi, featuring flexible digital interfaces. In terms of hardware, it adopts the RP2040 microcontroller chip independently developed by Raspberry Pi officials, is equipped with an ARM Cortex-M0+ dual-core processor, has an operating frequency of up to 133MHz, integrates 264KB of SRAM and 2MB of memory, and also comes with as many as 26 multifunctional GPIO pins on board.In terms of software, you can choose the C/C++ SDK provided by Raspberry Pi or use MicroPython for development. Supporting complete development materials and tutorials are also available, which facilitates quick getting started with development and embedding applications into products.

?code=NmE2MThhYzg2YzdhZDMzNTY0M2VlY2Q2OTBhY2Y4MzJfbjcwUnE4SWkwVkxMTUdUaU93OUU5QmZSQkVOSlZlSHRfVG9rZW46VzhZUmJiSEd3bzVSQ3F4SzR5dWN5RGNObk5jXzE3ODQ3ODk4NjU6MTc4NDc5MzQ2NV9WNA&add_watermark=true&scene_type=CCM

Figure 1.1 Front View of Raspberry Pi Pico Development Board

?code=MDIwNGM0ODBhNDEyNDA5ZDhhZTU1MjBlZDZiMzI4OGFfR3pMbTBrbWhOSUl3bHFGRVQ3VlZZTDRVV2p2dWlYSmlfVG9rZW46WDFuOWJhNE02bzlOOG94Y3d1cmMwZHFTbmhiXzE3ODQ3ODk4NjU6MTc4NDc5MzQ2NV9WNA&add_watermark=true&scene_type=CCM

Figure 1.2 Reverse side of the Raspberry Pi Pico development board

2. Hardware Circuit of Pico Development Board

Beginners can think of the RP2040 chip as "a phone motherboard without a screen, battery or buttons" — it has core functions, but cannot work without these accessories. These hardware circuits supplement the chip with essential functions such as "power supply, clock, status indicator and interfaces", turning the Pico from a "bare chip" into a "directly usable development board".

?code=ZWE5NjQyN2Y5ZDA0MjVkZWExZTkyNGRhZjc3YTM2NmVfczVpMWFyMUMwVk1yd1JldGVMcjdsMERCZllQbUM5OTNfVG9rZW46UUxCUmI3WGM0b2gwN2N4TWNVRGNMSWt3bnhkXzE3ODQ3ODk4NjU6MTc4NDc5MzQ2NV9WNA&add_watermark=true&scene_type=CCM

The Raspberry Pi Pico is equipped with some peripheral circuits of the RP2040 chip, including: an external Flash memory chip (W25Q16JV), a clock crystal oscillator, passive components such as power filter capacitors, a USB connector, a reset button, an LED, etc. Most of the available pins of the RP2040 chip are led out on both sides of the Pico development board, and four pins are used for internal functions, including driving the onboard LED, powering the development board, and selecting the BOOT mode, etc.

The schematic diagram of the Raspberry Pi Pico is shown below, which consists of an external clock crystal oscillator circuit, a BOOT mode selection circuit, a power supply input circuit, a power supply voltage measurement circuit, an LED indicator driving circuit, a debugging interface circuit, a pin expansion circuit and a chip peripheral circuit, and we will introduce them one by one next.

?code=MzhjZmM4OTc4Mzc1YzdiYzAyNzBmOTg1OTRmN2ZiYWVfa0hMd1VnZHJYUHp1WTNWaFNKbWppWWVkZjhaMUc1YllfVG9rZW46Q1U5QmJaNjBrb21GaWh4NlJGbGNFTkJobkRiXzE3ODQ3ODk4NjU6MTc4NDc5MzQ2NV9WNA&add_watermark=true&scene_type=CCM

Figure 1.4 Circuit Schematic of Raspberry Pi Pico Development Board

Simply put, the peripheral circuits of a Pico development board consist of the following parts:

  • Clock Crystal Oscillator Circuit: A circuit composed of a 12MHz crystal oscillator (labeled X1 in the diagram) and small components such as capacitors. It acts as the "metronome" for the chip — the chip's operations and communication with peripherals all rely on precise "timing rhythm", and this circuit delivers a stable "beat signal" of 12 million cycles per second to ensure the chip operates with accurate timing (for example, timing a 1-millisecond LED flash relies entirely on this beat to calculate time).

  • BOOT Mode Selection Circuit: Essentially, it is a small circuit equipped with a BOOTSEL button, serving as the "boot mode toggle switch" for the chip, which has two modes during startup:

    • Normal Mode: Launch the saved program;

    • BOOT Mode: The firmware flashing state is the "program loading mode" of Pico: after connecting Pico to a computer while holding down the BOOTSEL button, Pico will switch to this state (without launching the old program), and at this point it will be recognized by the computer as a storage device. Simply drag the written program (firmware) into it to install new functions for Pico.

  • Power supply input circuit: This is the circuit in charge of power management (such as the power chip U2 in the diagram). We can connect it to a USB (5V) or a battery (2-5V), and this circuit will stably convert the input voltage into the 3.3V required by the chips, as well as filter out the clutter in the voltage to prevent the chips from being damaged by sudden voltage fluctuations.

  • Power Supply Voltage Measurement Circuit: A small circuit designed to detect the power supply voltage. It acts as the "built-in voltmeter" of the board, capable of measuring the input power voltage in real time (for example, when powered by batteries, it lets you know if the batteries are running low), making it convenient for you to monitor the power status.

  • LED Indicator Driver Circuit: A small circuit that controls the onboard LED; the chip can turn this LED on/off via the GPIO25 pin to indicate status (e. g., blinking when the program is running, steady-on when power is connected).

  • Debug Interface Circuit: This refers to the DEBUG header (3-pin header) shown in the diagram, which serves as the "fault diagnosis port" of the board. If your program is corrupted or the board fails to operate, you can connect a debugging tool to this interface to check the internal operating status of the chip and pinpoint where the program has gone wrong.

  • Pin Extension Circuit: A circuit that configures chip pins into header pins (labeled CON_PICO_40W in the diagram). The pins on the RP2040 chip itself are too small to directly insert wires; this circuit extends the chip pins into header pins, allowing you to directly insert DuPont wires into these headers to connect external components such as sensors and motors.

  • Peripheral circuit of the chip: A circuit composed of small components such as filter capacitors and resistors around the chip. For example, filter capacitors can filter out the clutter in the power supply to make the power supply for the chip more stable; resistors can protect the pins from being burned out by excessive current, and prevent the chip from malfunctioning due to external interference or current fluctuations.