Skip to main content
JOrta
Associate II
Jul 11, 2019 6:39 PM UTC
Question

Does having a coin cell battery give a significantly quicker fix?

Is there a significant improvement in having a fix quicker by having the coin cell battery?

or can i live without it..

This topic has been closed for replies.

1 reply

ST Employee
Jul 12, 2019 6:37 AM UTC

Hi

VBAT (supplied with coin cell battery) manages the internal SRAM and RTC.. they are used to validated or not the previous dowloaded satellite data.

At the end if in your design you plan to swtich_off VCC/VCC_IO and you want avoid a cold-boot on each repowering the VBAT supply (coin cell battery) is mandatory to guarantee a TTFF of 4s instead of 32s.

Hope this helps.

Regards

Francesco