Skip to main content
Associate
Feb 4, 2026 10:30 PM UTC
Question

DC on RFin on LIV4F GPS Module

Is there a way to turn the DC off on the RF_IN port on the LIV4 GPS module?  There must be an enable or disable feature available via firmware.  Thanks for reading.

Scott

3 replies

ST Technical Moderator
Mar 5, 2026 5:00 PM UTC

Hi,

The capability to turn off DC bias in RF_IN line on LIV4F is not provided.

May I ask what is the use case for having this off? Is it trying to connect an active antenna with different input voltage?

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
shootenAuthor
Associate
Mar 5, 2026 5:23 PM UTC
We're supporting LIV4 and LIV3 on the same board and have an L1/L5 LNA in
front of the device. The DC is causing problems for us. We do not use an
active antenna. Thanks for the reply.
ST Technical Moderator
Mar 5, 2026 9:46 PM UTC

Ok, the RF signal chain is slightly different for LIV3F and LIV4F. 

In this case you might have to put a blocking capacitor in front of LNA.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.