Skip to main content
Dror
Associate III
Dec 1, 2019 11:06 AM UTC
Question

Bring up of new platform using TeseoIII

I am trying to bringup a new platform with TeseoIII.

I manage to flash the firmware, erase etc. However, when using Teseo-Suite, i can see 1-2-3 satellites recognized and a short few seconds after being visible on the Signal level window, they disappear.

Are you familiar with this behavior? What could be the cause?

    This topic has been closed for replies.

    2 replies

    Dror
    DrorAuthor
    Associate III
    Dec 1, 2019 2:10 PM UTC

    Found root-cause.

    A small 0201 size ferrite-bead was used in series to VINL1 power input. This caused a drop in 1.8V supply when GNSS engine started to work towards a fix, this probably caused the internal engine to reset.

    Replaced the bead with 0 ohm. Issue resolved.

    ST Employee
    Dec 2, 2019 8:14 AM UTC

    Perfect.

    Less work for me ;)

    For any question feel free to ask.

    If you can could you share some info on your TeseoIII project (you can write me directly francesco.virlinzi@st.com)

    Thansk

    Regards

    Francesco