Skip to main content
David Littell
Senior II
Jun 9, 2026 2:26 PM UTC
Question

Whither Dark Mode?

It would be nice if the new forum provided Dark Mode.  The new one somehow even prevents Dark Reader (under Safari) from working correctly.  Dark Reader worked fine on the old forum platform, so imagine my surprise…   😳

10 replies

Lina_DABASINSKAITE
ST Community Manager
Jun 9, 2026 2:34 PM UTC

Hi ​@David Littell ,

Do you have the same experience on different browsers as well or it’s only Safari? 

Meanwhile, I am checking what’s the expected behavior.

Thanks, 
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
David Littell
Senior II
Jun 9, 2026 9:11 PM UTC

The Dark Reader extension/plugin/whatever I’m using with Safari is a paid-for app so I don’t have it for any other browsers.

 

Thanks,

Dave

 

Lina_DABASINSKAITE
ST Community Manager
Jun 10, 2026 1:39 PM UTC

Hi ​@David Littell , 

I checked and I got confirmation that this is expected behavior.

I have raised and enhancement request and it’s under review with our vendor.

At this point, I cannot give you a timeline for the implementation.

Feedback from other users is also welcome to help assess the feature's importance.

Kind regards,
Lina


 

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
MM..1
Super User
Jun 10, 2026 3:26 PM UTC

Compare your White light with , i mean work of the devil is no choice ...

 

David Littell
Senior II
Aug 12, 2026 2:38 PM UTC

I’d like to again request that dark mode be supported on ST forums.  These are the only forums I frequent that neither provide a native dark mode nor properly allows the Dark Reader extension to work.

AScha.3
Super User
Aug 12, 2026 4:29 PM UTC

I have Dark Reader  , extension, installed.

And Chrome , actual , in “dark mode” setting.

So no need, to wait for ST-forum “upgrade” . :)

 

If you feel a post has answered your question, please click on " Best Answer ".
David Littell
Senior II
Aug 12, 2026 5:28 PM UTC

I’m using Safari, thanks.

AScha.3
Super User
Aug 12, 2026 5:34 PM UTC

..so you could try:

  • Turn Off the Lights
  • GS Dark
  • Dark Night - mode for Safari

 

If you feel a post has answered your question, please click on " Best Answer ".