Skip to main content
Uwe Bonnes
Chief
May 1, 2024 12:25 PM UTC
Question

What is the timezone of this forum?

What is the time zone of the forum. My last complaint is tagged "2024-05-01 5:21:40 AM" while here it is about 12:23:34 UTC 2024.

 

Please tag the posting explicit with the tinmezone!

This topic has been closed for replies.

20 replies

Andrew Neil
Super User
May 1, 2024 1:06 PM UTC

I have never understood what timezone the forum is using!

It's certainly no timezone anywhere near the one I'm actually in (UK)!

 

EDIT:

It's tagged this as ‎06:06 AM - it's actually 14:06 BST here.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AScha.3
Super User
May 1, 2024 1:31 PM UTC

Ok, im not far away , Germany . Here summertime (+1h) , now 15:31 .

ed

forum shows 03:31 PM.

so we know... :)

ed2

AScha3_0-1714570402774.png

 

If you feel a post has answered your question, please click on " Best Answer ".
Andrew Neil
Super User
May 1, 2024 1:15 PM UTC

Also, if you're going to present times as, eg, "06:06" then the leading zero indicates that it's 24 hours - so the AM should not be there.

"06:06 PM" should never be seen! 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
May 1, 2024 1:33 PM UTC

Looks to be Pacific Time / California (GMT-8)

08:33 in Chicago, 06:33 in San Jose

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief
May 14, 2024 4:04 PM UTC

Any opinions on this subject from STM side?

Tesla DeLorean
Guru
May 14, 2024 4:29 PM UTC

Will be system default when not logged in.

 

@Lina_DABASINSKAITE @STTwo-32 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Lina_DABASINSKAITE
ST Community Manager
May 15, 2024 8:52 AM UTC

Hi @Uwe Bonnes ,

Thanks for raising this question and apologies for a delayed response. The default time zone of the forum is: GMT -08.00 U.S. Pacific Time. 

As @Tesla DeLorean correctly pointed out, the time zone can be adjusted based on your preferences via My settings > Preferences > Time zone.  At this point of time, it is not possible to automatically adjust the time zone display, for example: based on your defined location on a profile. 

I will check if there are any feature updates upcoming and get back. 


​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Lina_DABASINSKAITE
ST Community Manager
May 15, 2024 9:24 AM UTC

Hello @Andrew Neil @Uwe Bonnes , @Tesla DeLorean , 

To cover the additional points in the discussion: 
- The default time zone when logged out is the system one: GMT -08.00 U.S. Pacific Time.
- The one you set on your settings is only for the log-in view. 

@Andrew Neil , thanks for pointing out the incorrect formatting, I will check if it is an easy fix and get back. 

Greetings,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Uwe Bonnes
Chief
May 15, 2024 10:17 AM UTC

@Lina_DABASINSKAITE: So please tag the time with the correct timezone indicator!

Uwe Bonnes
Chief
Oct 25, 2024 5:33 PM UTC

Any news on tagging all dates with the timezone?