Skip to main content
Associate II
Jun 10, 2026 7:08 AM UTC
Question

subject line in email notification

I have some subscriptions around STM32 community and appreciate email notifications for it. This gives me many mails every day with only a few of them beeing really interesting for me. So I have a look on my incoming mails from time to time and want to have at least a short reading in a few interesting ones and delete the others immediately.

Before switching to the new forum SW I received emails for my subscription with a sender field reading Community Mailer and a useful subject line like e.g.:

Re: Floating point vs fixed point calculations (STMicroelectronics Community Subscription Update)

So I see could decide very fast which mails could be deleted immediately leaving only some of them to open for reading.

 

Now all notification mails have the same sender again of course entry (now ST Community notification) and nearly all the same subject line like A new topic has been created in STM32 MCUs Boards and hardware tools. (differing only in the subscription title).

The subject line gives me not more information than the sender field, I really miss the author’s subject line in my incoming mailings list.

 

This change renders the subscriptions conpletely useless for me since I will not open 100 or more mails a day just to find the one or two interesting enough (for me) to read.

 

Is there a chance to get a useful subject line again?

 

BR Klaus

12 replies

Lina_DABASINSKAITE
ST Community Manager
Jun 10, 2026 7:16 AM UTC

Hi ​@mfgkw ,

Thank you for sharing this feedback.

The way notifications are sent from this and the platform vendor before are out of the box and changes we could do are minimal.

I will check if there are more options available and get back.

Feedback from other users is also welcome to help assess the feature's importance.

Kind regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Jun 10, 2026 8:05 AM UTC

I also see notifications referring to “your thread”, when it is not my thread - just one I happen to have contributed to.

 

PS:

Here’s an example:

 

This is the thread:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Jun 10, 2026 8:33 AM UTC

Sometimes the messages do have useful subject lines:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Grant Bt
Associate III
Jun 10, 2026 8:58 PM UTC

I agree, this is a must-do. My most recently received message:

A new topic has been created in STM32CubeMX (MCUs)

whereas it should be

Differences between code generated for STM32CubeIDE and CMake

Or perhaps better?

[MCUs:STM32CubeMX] Differences between code generated for STM32CubeIDE and CMake

 

One of, or both categories would be nice, if terse.

Thanks,

GB

Grant Bt
Associate III
Jun 11, 2026 3:08 PM UTC

Before and After shots.

 

Grant Bt
Associate III
Jun 12, 2026 2:59 PM UTC

Sad to say, but this version of the forum has destroyed email subscription functionality by changing the Subject. Hopefully someone can fix this. I primarily read the forums via email as it’s much faster and easier to archive the content I want to save, and the old stuff I have survives changes like these. I do not want to scroll endlessly through web pages so unless I’m searching a particular issue. The community is lost to me for now.

Lina_DABASINSKAITE
ST Community Manager
Jun 16, 2026 1:52 PM UTC

Thanks for sharing ​@Grant Bt . We looking what is possible to do to change this. 

So far, the topic title is included in the notification about “Replies”. 

Kind regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Grant Bt
Associate III
Jun 17, 2026 3:26 PM UTC

Thanks for the tweak ​@Lina_DABASINSKAITE, I have enabled that now.

it looks like one can use Outlook to run a script as part of the Rules & Alerts feature (you have to enable the feature first). Then the script could parse the message’s first paragraph and modify the subject line. Not sure when I would have time to do this but one pathway is indicated here: SlipStick Systems: Rename Subject Line with Email Content

 

I confirmed that the option “run a script” can be made available in Outlook (possibly other email clients as well … Thunderbird?). Now I just need time to create a script!

 

Grant Bt
Associate III
Jun 18, 2026 7:28 PM UTC

This simple script works, but there is no RE: prepended to followups:

 

Public Sub ChangeSubjectFromBody(Item As Outlook.MailItem)     Dim bodyText As String     Dim phrasePos As Long, quoteStart As Long, quoteEnd As Long     Dim newSubject As String          ' Fetch the plain text body of the email     bodyText = Item.Body          ' Look for the anchor phrase     phrasePos = InStr(1, bodyText, "posted a new topic")          If phrasePos > 0 Then         ' Find the opening quote character after the anchor phrase         quoteStart = InStr(phrasePos, bodyText, """")                  If quoteStart > 0 Then             ' Find the closing quote character after the opening quote             quoteEnd = InStr(quoteStart + 1, bodyText, """")                          If quoteEnd > quoteStart Then                 ' Extract the text between the quotes                 newSubject = Mid(bodyText, quoteStart + 1, quoteEnd - quoteStart - 1)                 newSubject = Trim(newSubject) ' Remove accidental spaces                                  ' Apply and save the new subject line                 If Len(newSubject) > 0 Then                     Item.Subject = newSubject                     Item.Save                 End If             End If         End If     End If End Sub

 

Lina_DABASINSKAITE
ST Community Manager
Jun 19, 2026 12:03 PM UTC

Thanks for sharing this ​@Grant Bt ! I am happy to see you found a solution to the inbox look in the way you want.

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.