Skip to main content
TDK
Dec 8, 2023 9:04 PM UTC
Solved

Should I be reporting AI-generated nonsense responses?

In instances where they don't answer the question, or where they answer it incorrectly, I have been reporting these. Should I keep doing so?

Does the ST community have a stance on whether or not AI-generated reponses are allowed? Is that stance in the guidelines and if not, can we put it there?

For example, clearly this is ChatGPT generated nonsense:

TDK_0-1702069354794.png

Another one, same thread even.

TDK_1-1702069376813.png

At first glance it seems like these answer the question, but they fall apart under inspection. These two are obvious, some are less so.

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Dec 9, 2023 8:22 PM UTC

    @TDK @waclawek.jan 

    Thank you very much for reporting AI generated spam! We are now able to automatically block and remove a lot of URL posting spammers. But recognising AI spam interspersed in threads is still a challenge from time to time.

    We are happy to receive reports from users of the respective threads, who should now also be informed by the community by email if this is allowed in their settings.

    Thanks again and happy hunting spam!

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    22 replies

    waclawek.jan
    Super User
    Feb 10, 2024 10:09 AM UTC

    @Laurids_PETERSEN, not related to this thread materially but related to Andrew's above suggestion, can the list also contain "not inappropriate content, but in inappropriate forum" option (i.e. a suggestion to move given thread to a more appropriate place)?

    Thanks,

    JW

    Andrew Neil
    Super User
    Feb 10, 2024 10:42 AM UTC

    @waclawek.jan wrote:

    can the list also contain "not inappropriate content, but in inappropriate forum" option (i.e. a suggestion to move given thread to a more appropriate place)?


    +1

    :thumbs_up:

    As with AI stuff, I currently put that under 'Something else'.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Lina_DABASINSKAITE
    ST Community Manager
    Feb 28, 2024 10:20 AM UTC

    Hello @Tesla DeLorean , @waclawek.jan , all, 

    I want to assure that all abuse reports we review daily and take respective actions.

    For all other reasons and that are not falling under the suggested ones, choose "Something else" and provide a short action/comments you think is necessary and we will take it further. 

    I am looking into possibility to add a couple of personalized reasons but can not promise you when and how this could be implemented. I will get back once there are more news on this. 

    Thanks a lot for your contributions on this topics,
    Lina

    ​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Andrew Neil
    Super User
    Apr 28, 2025 5:17 PM UTC

    @Lina_DABASINSKAITE wrote:

    I am looking into possibility to add a couple of personalized reasons but can not promise you when and how this could be implemented. I will get back once there are more news on this. 


    Another one for that list: "Question is about xxx Pill" !

    See: https://community.st.com/t5/feedback-forum/why-you-are-lock-the-chat-without-give-solution/td-p/797229

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.