Skip to main content
TDK
Jul 9, 2025 4:05 AM UTC
Solved

Reply to a post has gone missing

I replied to this thread previously:

https://community.st.com/t5/stm32-mcus-embedded-software/errors-building-gpio-exti-example-project-for-the-stm32f746zg/m-p/820361#M65664

 

My reply was the 2nd post, just before Pavel's. My post is now missing or deleted. What happened to it? It was there for quite a few days before disappearing.

TDK_0-1752033964183.png

 

I don't think anything nefarious is happening, but this happens every so often and I'd like to get to the bottom of it. I don't have permissions to delete posts, so I don't think it wasn't anything I did. Did a spam filter pick it up? Did a mod or admin accidentally delete? Do community admins have suitable permissions to figure out this mystery? Was the thread moved and my post missed the bus somehow?

This topic has been closed for replies.
Lina_DABASINSKAITE
ST Community Manager
Jul 15, 2025 10:17 AM UTC

Hi @TDK 

It was a not intended content move done by one of our moderators. Instead of moving a thread, a single reply was moved. This can happen due to replies having different URLs than a main thread.

I’ll use this as a chance to brief the team on the process once again and the importance of notifying in the correct way. 

Apologies for this and thanks a lot for reporting.

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

Tesla DeLorean
Guru
Jul 9, 2025 5:12 AM UTC

>>.. but this happens every so often and I'd like to get to the bottom of it

Yeah, I get this deja-vu feeling on occasion, where I can swear I replied to a thread, but I can't find it.

It perhaps didn't register, or I got distracted and closed a tab. I also see on occasion where Reply on the Phone is near the Feedback tab on the right side, and I have to scroll the screen so the Reply is distinctly separated and I can press it AGAIN for the post to be accepted / registered.

Other times I suspect the top-post gets moved, or edited, as I type a response, and this messes things up, or flags the thread/post doesn't exist when hitting REPLY.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Lina_DABASINSKAITE
ST Community Manager
Jul 9, 2025 9:15 AM UTC

Hi @TDK , 

Thanks for reporting. I found your post moved out as a stand-alone post in the same forum board and moved it back to the thread. See it here: Re: STM32 Failure to Build - STMicroelectronics Community 

Seems that it was an accidental move by either one of the super user or moderators (only those people have the rights). I will have to check the logs and get back once I find out. 

Regards,
Lina


​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
TDK
TDKAuthor
Jul 9, 2025 3:18 PM UTC

Thanks @Lina_DABASINSKAITE . I got an email notification when you moved it back, but I didn't get any notification when it got moved originally, as I normally do when threads get moved.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Lina_DABASINSKAITE
ST Community Manager
Jul 15, 2025 10:17 AM UTC

Hi @TDK 

It was a not intended content move done by one of our moderators. Instead of moving a thread, a single reply was moved. This can happen due to replies having different URLs than a main thread.

I’ll use this as a chance to brief the team on the process once again and the importance of notifying in the correct way. 

Apologies for this and thanks a lot for reporting.

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.