Skip to main content
unsigned_char_array
Lead III
Jul 1, 2026 9:31 AM UTC
Question

Notification does not open the referenced post

Related but different topic:
 

 

I got a notification of a new post, but clicking on it didn’t bring me to the last post. I scrolled down to find the post and did not see it. I did ctrl+f to find the post by username and got the reply. It was very high in the thread. My beef is they are not chronological. But it’s also an issue that clicking on the notification did not take me to the post initially. I can’t reproduce that anymore.

    6 replies

    Lina_DABASINSKAITE
    ST Community Manager
    Jul 1, 2026 3:42 PM UTC

    Hi ​@unsigned_char_array , 

    Can you please share screenshot / video of the notifications you received and where you are redirected once you click on them? Please also include relevant URLs. 

    This would help a lot on troubleshooting. 

    Thanks,
    Lina

    ​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    unsigned_char_array
    Lead III
    Jul 1, 2026 4:06 PM UTC

    They are in the topic I posted this in.
    I don’t understand why my post was moved outside the topic. Please put it back. There are already 2 related, but different topics. Now there are 3 topics. And I cannot edit my post either

    "Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
    Andrew Neil
    Super User
    Jul 1, 2026 3:55 PM UTC

    Pretty sure I’ve seen this, too.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    Jul 10, 2026 9:42 AM UTC

    Pretty sure I’ve seen this, too.

    Example just now:

     

    When I click that notification, it gives me this:

     

    So the post at the top of the page is not the one which the Notification referred to.

     

    (When I originally clicked this, I’m sure that the referred post wasn’t even visible - this does seem to be a bit random)

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Visitor II
    Aug 12, 2026 1:39 PM UTC

    The notification should take users directly to the referenced post. In long threads, having to manually search for the reply defeats the purpose of the notification. Combined with non-chronological replies, it makes following discussions unnecessarily difficult.

    For more details, visit here: https://community.st.com/feedback%2Dforum%2D118/option%2Dto%2Dshow%2Dreplies%2Dchronologicallink%2D166576

    Andrew Neil
    Super User
    Aug 12, 2026 2:15 PM UTC
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.