Skip to main content
dungeonlords789
Associate III
Jun 11, 2026 6:12 AM UTC
Question

New community platform: markdown feature

I am sad that I can’t use markdown in community.st.com To be honest, I am interesting in the only one feature: codeblock. I think that ``` or ```bash is very convenient and became industry standard. Even Telegram messenger supports it. Do you plan to add markdown codeblock style? It is weird to click on the … and click to “Code” item in menu… Are we on technical forum? Why we have quick access to Text color but not to codeblock? I feel like new community.st.com comes from outsource designer which really don’t understand content of the forum.

    4 replies

    Andrew Neil
    Super User
    Jun 11, 2026 7:52 AM UTC

    ​@dungeonlords789 

    I am sad that I can’t use markdown in community.st.com 

    That was also the case with the previous forum

     

    It is weird to click on the … and click to “Code” item in menu…

    It has already been accepted that this needs changing:

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Lina_DABASINSKAITE
    ST Community Manager
    Jun 11, 2026 1:51 PM UTC

    Hi ​@dungeonlords789 , 

    Thanks raising this up. So far there no plans to add it. 

    Feedback from other users is also welcome to help assess the feature's importance.

    Thank you,
    Lina
     !--endfragment>!--startfragment>

    ​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Andrew Neil
    Super User
    Jul 14, 2026 1:14 PM UTC

    Quite a few people do seem to be assuming that the forum will support it; eg,

     

    And note that there is currently no way to post “preformatted” text which is not source code:

    This was available in the old forum.

     

    However, I do note that the Code Editor here lists ‘Markdown’ as a language option:

     

    Let’s try it:

     

    In the composition window, it looks like this:

     

    Here it is:

    ```text
    1: Yippie (BSSID: 3C:A6:2F:B5:E4:37, Kanal: 11, RSSI: -48 dBm)
    2: RAK7268V2_BAD1 (BSSID: AC:1F:09:19:BA:D2, Kanal: 11, RSSI: -50 dBm)
    3: Yippie (BSSID: D4:24:DD:4D:F2:2F, Kanal: 11, RSSI: -54 dBm)
    4: Yippie (BSSID: DC:39:6F:1F:5C:03, Kanal: 11, RSSI: -76 dBm)
    5: linksys (BSSID: 98:FC:11:CE:00:16, Kanal: 9, RSSI: -86 dBm)
    6: Yippie (BSSID: D4:24:DD:4D:F4:90, Kanal: 11, RSSI: -86 dBm)
    ```

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    Jul 14, 2026 1:17 PM UTC

    Here it is:

     

    And now a screenshot of how that appears:

    So it does give us monospaced text, but still with the markdown tags.

    And line numbers - which may or may not be a good/useful thing.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.