Skip to main content
waclawek.jan
Super User
Jun 18, 2023 8:29 PM UTC
Question

Insert emoji does not work.

Insert emoji:

waclawekjan_1-1687120091638.png

does not work.

I don't miss it - contrary, I call for removing the unnecessary stuff like this.

We don't need Comic Sans either, if you know what I mean.

JW

This topic has been closed for replies.

17 replies

Jun 19, 2023 3:40 PM UTC

Hello @waclawek.jan ,

I moved this here from: 
Solved: Forum migration lost code formatting - STMicroelectronics Community for a better problem visibility as we want to avoid multiple topics in one thread.

Thanks for reporting this question. We are looking into the emoji situation already. Regarding the Comic Sans, noted but need more votes on this one to pass :D 

BR,
Lina - ST Community Team (New profile @Lina_DABASINSKAITE )

Peter BENSCH
ST Technical Moderator
Jun 24, 2023 8:12 AM UTC

+ no for Comic Sans

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
waclawek.jan
Super User
Jun 19, 2023 9:33 PM UTC

:D

 

waclawek.jan
Super User
Jun 19, 2023 9:35 PM UTC

Hey! My smiley got censored!I do have nose! I don't like my smileys to be mutilated!

JW

test, all with noses: :) :D ;)

 

Amelie ACKERMANN
ST Community Manager
Jun 23, 2023 8:58 AM UTC

Hello @waclawek.jan,
We can enable/disable the insertion of emojis via the admin settings. I have now enabled it - I understand you disagree, but other members might wish to use emojis as it is a very common part of written communication nowadays. Let's now see how the community makes use of emojis and take it from there. 

Best,
Amelie

waclawek.jan
Super User
Jun 23, 2023 12:05 PM UTC

Hi Amelie,

If "disabled" means "the icon is there but it does not work", then enabled is certainly better.

However, I don't like the forum to change the manually written smileys, e.g. the following basic smiley was written as colon dash right bracket: :)

You may find this to be pickiness, but there is an actual reason for this: in technical texts we use, combinations of non-alphabetical characters including colons and dashes and brackets occurs quite often. And "features" like these mutilate that text, too.

This again is something well understood by real forum software writers, and I see why the newfangled script kids in Khoros and alike find it amusing and don't understand that it just gets into way. I can't stress enough how frustrating small but important things like these gets into way and spoil one's day. So, just don't. If you must have emojis, insert them as images.

JW

Amelie ACKERMANN
ST Community Manager
Jun 29, 2023 7:18 AM UTC

Hello @waclawek.jan, 

Thanks, I understand your point. Emojis within preformatted text are turned off. Have you had issues in your technical texts, nevertheless? 

Best,
Amelie

 

 

waclawek.jan
Super User
Jun 23, 2023 1:09 PM UTC

Alternatively, use Unicode emojis: :grinning_face:

JW

waclawek.jan
Super User
Jun 24, 2023 7:59 AM UTC

Enabling emojis was maybe not the best idea.

Now it takes quite forever (25 sec) for a page to load, and quite a bit of data are transferred.

waclawekjan_0-1687593584436.png

 

Emojis for the masses. A worthy goal, is it.

JW

waclawek.jan
Super User
Nov 22, 2023 9:29 AM UTC

This is still a problem and loading the 1500 pngs simply takes forever, for exactly zero benefit.

This is a technical forum, not a chitchat.

Just switch them off.

JW

@Amelie ACKERMANN 

@Laurids_PETERSEN 

Laurids_PETERSEN
ST Community Manager
Nov 22, 2023 10:02 AM UTC

Hi @waclawek.jan, 
Thanks for reaching out again.

We will discuss the performance impact of having emoji's enabled again internally.
Other options to explore could be to stop a preload of the emojis, unless the emoji component of the text editor is used, or to implement Unicode instead. 

I will keep you posted on which direction we are taking with this matter. 

Best regards, 
Laurids

waclawek.jan
Super User
Nov 30, 2023 5:30 PM UTC

Hi @Laurids_PETERSEN ,

I've disabled them locally long ago so can't judge the improvement.

Probably better, but I maintain that they are not needed at all. Technically savvy users can type a colon and a bracket when they need to. (And automatically correct that character combination is inappropriate, either, test, :) :( :) :( ;) :Dto cite a few

Oh, it's even more idiotic than expected. I typed an assortment of normal character smileys above, maybe half a dozen different ones, with and without nose. It threw an "invalid HTML", then upon repeated click on Post it converted *some* of them to images, and during edit it removed *all* of them and upon posting the edit - which was only adding this text without touching the smileys - it removed the converted images... I'm not going to investigate further, I don't care.).

I mean, whatever you do, this won't make it an appropriate forum anyway. Smileys and stuff we and you waste time and energy here are just the insignificant tip of the iceberg. Try to read my comments I gave to your colleagues.

JW

 

waclawek.jan
Super User
Jan 17, 2024 10:17 AM UTC

I've been bitten by the idiotic autoconvert again, trying to type number eight and a closing bracket. Oh, c'mon.

JW

unsigned_char_array
Lead III
Feb 3, 2025 1:50 PM UTC

Button still doesn't work. Either fix it or remove the button.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."