Get ready for the STM32 Summit 2026 | Online, November 3
Raise questions or provide feedback on our community platform.
Most recent activity
When trying to post, I get an assortment of problems: an edit pane into which I can't write; various red warnings when trying to preview or send the post, etc.I presume this is exposed as consequence of the "permanent reload on FF" problem: I click on "stop loading" icon to prevent the permanent reloads, and probably some of the magic javascriptoids won't load. Nonetheless, this may happen also if users for any reason click on the "stop loading" icon of browser during the first loading of the page, or some of the files simply won't load, e.g if using a slow and intermittent internet connection (yes, not everybody has top notch internet connectivity all the time, and yes, that should've been part of the testing).There's no remedy to this problem except to ditch Khoros and get a decent forum software. Yes, I know it came quite soon.I wonder if you've tried it on FF at all by now.JW
There are many threads where users have been unable to attach IOC files. Here is one of them:https://community.st.com/t5/stm32-mcus-products/uart-cannot-set-high-baud-rate/m-p/621673#M230659 The IOC file type is clearly not a security concern. Is there some other reason they are blocked or is this just an oversight? Can we get it corrected? Edit: I have no problems attaching an IOC file. So is this a permissions issue? New users can't attach files or something? I would say even a first time user first time poster here should be able to. Coming to a forum to ask for help and including the relevant file seems a very reasonable thing to do. Cheers.
Hi all,I´posted a shutdown issue with the L4981A controller and unknowingly the profile page had broken content and didn´t provide all the details. As such I got a reply with a case number from an St employee requesting my company info (which was already given) in the profile site, but have heard nothing since. Has this "dried up" ? I tried to access the profile site but the page didn´t open. All I get now from mySt is more login details on top of the one already given ! and a blank page getting no where. It has taken me 1/2hr to get to this forum. Browser firefox, otherwise a relatively new notebook.All very disappointing. Time for customers to be better looked after.rJ
Answers to other ones posts are placed directly under the posts. This is unusual to most other forums. I dont know if i like it or not. But at least should be clearly(!) visible, that this is an answer. Use an indentation? Also its kinda confusing to have a solution to appear twice in the thread.There are so many things a developer has to read through. Please dont make it harder with a confusing forum.
Can we have more than 5 posts displayed at once in user's User Activity list? For example the same number as the number of threads displayed in forums views (as it's substantially the same amount of information, and it's user settable, somehow, somewhat)?Thanks,JW
JW
Incidentally, if Firefox browser Privacy and Security -> Do Not Track set to Always, then it is not possible to reply to posts here. Nor does the Accept as Solution option appear.
When a link is given to a particular post and the post has a file attached, two horizontal lines appear under the small file icon.https://community.st.com/t5/stm32-mcus-products/stm32f4-hardfault/m-p/604656/highlight/true#M226598As can be seen in the picture, the lines do not appear on other posts with file attachments. And, if one takes a link to the second post of the two, then the lines appear on the second post but not on the first one.
what-the-huck-is-that?!!! my dear ST!you think you software is well-designed, works stable and correctly not because it isn't FULL OF BUGS and was never created DEFECTIVE-BY-DESIGN, but because you are not getting the feedback.the Suck-o-Sales era has become... and you know what? - there are Chinese guys, producing replacements of ST MCUs.am i really right in buying yours?
JW
The "member callout bubble" remained stuck even after having made the post i.e. editor pane closed. It overlaps the post and scrolls together with it.Oh yes, reload "fixes" it, but ain't it a hillarious fail?JW
I got a notification, where actually there is NO answer!
Here's a thread:https://community.st.com/t5/stm32-mcus-products/nucleo-144-no-pins-in-cn11-and-cn12/m-p/612257Here's what the top of the page looks like. Note that the "accepted solution" shown doesn't have the green border, and doesn't appear to have been selected by the OP as the answer.Another solution below does have the green border and appears to be the correct "solution" per the OP.Note that the "Go to solution" link goes to the incorrect solution.
Hi, @Amel NASRI ,now, that the Ideas are gone, can we please have back the annual Wishlist thread?Thanks,Jan@Amelie ACKERMANN, @Lina_DABASINSKAITE , @Laurids_PETERSEN
This page Free Arm Keil MDK for STM32C0, STM32F0, STM32L0 and STM32G0 - C/C++ Compiler, IDE/Debugger, CMSIS components, RTOS for STM32C/F/L/G/0 - STMicroelectronics and the rabbit hole it goes down is too deep and unnecessarily difficult to navigate to find the PSN / LIC that's needed Turns out it's here Keil MDK | Keil MDK for STM32 – Arm Developer (arm-sc10xp1-pre-prod-cd.azurewebsites.net)And the Product Serial Number good until December 2032 is 4RMW3-A8FIW-TUBLG
We should have a room for notable quotes somewhere.This one made my day today: There is an issue somewhere, but if we always fall back to "well it works on an identical configuration" we don't advance the ball.-- @TDK
Actually, there is text next to that icon. And it even highlights upon mouse hover, making it marginally readable.Congrats to modern feel and look.JWPS. Text ought to be BLACK and WHITE. Leave modern feel and look to marketing material. We actually need to read this.
How can I get a more Classic Forum view, say just the Subject/Title, like an email client, where I can see 50 posts, perhaps 25 to the physical height of the screen? Posting to main "Board" as there isn't a selection for "About Forum" or more appropriate venue. Also no appropriate "Label"
Dragged a mouse accidentally over this post down there. Pressed at least one or both of the left/right mouse buttons at the same time. The screenshot has not been modified...The only interaction with the page, that still works:Scrolling. Also middle (wheel) click does only scrolling anywhere on a page and doesn't open links in a new tab, like it normally does.Ctrl+A (select all). The left click cancels the "select all", but cannot do anything else.Right click.Happened on a Vivaldi browser, which is Chromium/Blink based.
Yesterday, the thread view changed from showing about 3 threads per page to about 10 or so by only showing the title and not a preview of the contents. It is so much better. It's something that has been suggested by myself and others multiple times. So thanks for that.I'm hoping this was a deliberate change and won't be changing back.I think it also shows users that the title matters so they should be more incentivized to pick a good title rather than something like "XYZ doesn't work". Glad we don't have many posts with the entire post in the title anymore.Progress.
I have to make this post, as it is really annoying for me. I would like to use other words for this, but im trying to stay professional about this!Its already bad enough, when your login expires after only like 1-2 hours. Now why on earth would a password expire, when i tried 4 times??? I am happy to wait an increasing few seconds after each fail. I guess when it expires, i cant reset it to the old one!?!Is it really necessary for the password, to have a requirement for 12 characters? And all the other requirements? What comes next? Two factor authentication?This is not a banking account!
When looking at a subforum, on the right side there are many labels available. For example, for the "Embedded software (MCUs)", the list starts with a label "ADC". But, when creating or editing a topic, there are just 9 labels available starting with "STM32Cube MCU Packages". Adding a valid label manually, ends up with an error message: "The following labels are not available here: ...".
This is not a bug of the forum engine, but of the main ST web server! Let's open the following link:https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdfBy default on a Chromium/Blink based browsers it just opens a PDF file in a tab, but on Firefox it offers a file download. The cause of the difference is the HTTP Content-Disposition header. Look at what a valid syntax is and what the ST web server returns:content-disposition: /resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdfThis is a nonsense, which doesn't conform to the HTTP standard! Apparently the Chromium/Blink based browsers interpret such a nonsense as "inline", but the Firefox interprets it as "attachment". Read the following link for a more detailed explanation and an override workaround for Firefox:https://support.mozilla.org/en-US/questions/1387228
If one takes a link to a specific post, then the posts, which had been moved from other topics, show the title of their respective original topic.Original post (OK)Moved post (wrong title):Also, as I have reported previously, adding a "Re: " in front of the title, is an anachronism from the e-mail "traditions" and is not only useless, but also worsens the usability.
I hate when i have to come on this site for resources.Now i need to download https://www.st.com/en/embedded-software/stsw-wise-studio.htmlBut it just does'nt work as i keep being repeated I have to log in but i already am. I tried switching browser.Nothing works, and i've lost so much time already :(Stress and money loss for me, thank you.
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.