Skip to main content
Jack3
Senior
Jun 30, 2026 5:55 PM UTC
Question

How can I edit my post after submitting? There's no edit option anymore?

How can I edit my post after submitting? There's no edit option anymore?

8 replies

Peter BENSCH
ST Technical Moderator
Jul 1, 2026 6:52 AM UTC

It should be possible to find the Edit function under the menu with the three dots at the top right of your post.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Lina_DABASINSKAITE
ST Community Manager
Jul 1, 2026 2:07 PM UTC

Hello ​@Jack3, 

The edit option is open for 60min after the post has been created. After that, this option is no longer available. 

Kind regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
unsigned_char_array
Lead III
Jul 6, 2026 12:03 PM UTC

Why 60 minutes? Why not 60 days? Is it temporary or permanent? I frequently edit my posts with improved formatting, spelling/grammar, and extra context. In fact I think I edit most of my posts several times.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Andrew Neil
Super User
Jul 1, 2026 2:20 PM UTC

As the others have said, you should be able to edit your own post - via the menu at top-right of the post:

 

But you can no longer edit the title:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Lina_DABASINSKAITE
ST Community Manager
Jul 2, 2026 1:09 PM UTC

​@Jack3 , If you need to edit content past 60min, you can Report the message and share the changes that needs to be done. 

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Jul 22, 2026 8:58 AM UTC

See also:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Aug 12, 2026 2:51 PM UTC

See also:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.