Skip to main content
unsigned_char_array
Lead III
Jul 15, 2026 8:24 AM UTC
Question

Hard to write text after image

I find it hard to write text after I inserted an image. Especially between two images.
I end up writing nonsense text first as a placeholder and inserting the images around that. Then I edit the placeholder text.
The old forum had a html view where you could easily place the blinking cursor after the image closing tag.

For example it is hard to put text under the first image:

 

The cursor can only be set to the image caption below the first image:

So then I need to delete the second image first to get in between.

I also don’t see the option to set image size anymore. Is it always full size?

2 replies

Andrew Neil
Super User
Jul 15, 2026 9:37 AM UTC

Yes, I have noticed this - it is, indeed, a pain.

 

I also don’t see the option to set image size anymore

Already noted:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Zita LASZLOFI
ST Community Manager
Jul 24, 2026 6:20 PM UTC

Thank you for sharing your experience with adding multiple images, ​@unsigned_char_array, and ​@Andrew Neil for adding your input. 

It is indeed not ideal, however, I believe it is current platform functionality. We are sharing this as well with our platform provider to see if we can improve this. 

Kind Regards, 
Zita
 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.