Skip to main content
unsigned_char_array
Lead III
Apr 24, 2024 9:29 AM UTC
Question

Forum bug: code snippet changes after editing post

If I have the following code snippet:

 

 

@Echo OFF

 

 

And I edit my post it changes to:

 

 

 OFF

 

 

In addition after edition the post it will add extra new lines around the snippet for each edit.

Syntax highlighting is good, but I'm missing a plain text option in case the language is not listed.

This topic has been closed for replies.

6 replies

Andrew Neil
Super User
Apr 24, 2024 9:34 AM UTC

@unsigned_char_array wrote:

 after edition the post it will add extra new lines around the snippet for each edit.


Yes, this is annoying.

 


@unsigned_char_array wrote:

missing a plain text option in case the language is not listed.


Absolutely!

There is often a need to have just monospaced plain text - no syntax highlighting.

eg, build output; ASCII Art

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Apr 24, 2024 9:35 AM UTC

Just trying it:

@Echo OFF
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Apr 24, 2024 9:37 AM UTC

@Andrew Neil wrote:

Just trying it:

 

@Echo OFF

 


This is what I actually entered:

AndrewNeil_0-1713951361998.png

So, in my case, it still shows the "@Echo" - but it's changed the case!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
unsigned_char_array
Lead III
Apr 24, 2024 9:43 AM UTC

Yes with me it changed the case too. It was all caps when I entered it. I think it confuses it for a username as the at symbol is used to reference users. But that should be ignored inside a code block. And with subsequent editing the at and the Echo will both disappear leaving the space and the off.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."