Skip to main content
DungeonLords
Associate II
Jul 9, 2026 11:00 AM UTC
Question

Allow dislike

I suggest to allow like and dislike votes. Dislike is important to indicate that the post contains wrong/weird information or working but not good technical decision. This is how best practices work.

2 replies

Andrew Neil
Super User
Jul 9, 2026 11:16 AM UTC

The trouble with this is that it can (and does) get abused; eg, as a grudge against the poster - rather than a comment on the content.

Also, just a “dislike” doesn’t tell what is wrong with the content.

 

to indicate that the post contains wrong/weird information or working but not good technical decision

Probably best to address that in a reply ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
unsigned_char_array
Lead III
Jul 9, 2026 11:46 AM UTC
  • I generally agree with allowing dislike buttons, but I don’t think the ST forum is the right place for it.
  • On social media you want to rate public posts/videos and individual comments and look at the ratio.
  • Here I occasionally upvote a comment when a user has a good idea or the same problem to highlight that comment. And I never had the desire to downvote.
  • ST forum posts don’t get many views on average, so the ratio becomes unreliable anyway
  • If the post is in violation of the terms it should be reported.
  • If you disagree with the contents you can just reply and explain why you disagree.
  • Even stackoverflow encourages adding a comment under a question or an answer before downvoting.
  • The previous forum didn’t have a dislike feature either. If it was and it was used heavily I’d understand the reason to preserve it.
"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."