Skip to main content
AAli.2
Associate II
Jul 17, 2024 1:38 PM UTC
Question

X-CUBE AI PROBLEM WITH INFERENCE RESULT

I have created my own cnn model and want to run it on STMH753ZI board using X-CUBE-AI. I have executed all the steps to run the inference. The inference is also running but the output is always 0. With my fixed input of sample shape (1,50,12). I cannot understand the problem. I attaching the code script and the terminal output.

 

 

 

 

 

This topic has been closed for replies.

7 replies

fauvarque.daniel
ST Employee
Jul 17, 2024 3:35 PM UTC

You can use the validate command on host or on the target to verify that your model is behaving the same way in Python and in C.

Generally it could be a problem with the way you pass the data to the network especially when the network is quantized.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AAli.2
AAli.2Author
Associate II
Jul 18, 2024 9:15 AM UTC

I have validated on desktop and on target. It validates successfully on system but give an error when validating on target.
Running the Keras model... 
Running the STM AI c-model (AI RUNNER)...(name=cnn, mode=TARGET) 
INTERNAL ERROR: E801(HwIOError): Invalid firmware - COM9:115200

Whereas COM9 is the port that I use to run the inference on board with output on Putty terminal which it does. 

I am attaching the screenshot of validation as well. I try to give the input in the same way as well as I see in validation like a 3d array to get shape (1,50,12). But doesn't seem to work. 

fauvarque.daniel
ST Employee
Jul 18, 2024 11:57 AM UTC

One way to see if the validation program is starting correctly on the board is to launch a pseudo tty on this com port and see if you have messages coming from the validation program when you reset the board (reset button).

If you have no messages the compile / flash of the program did not happen or did not finish successfully

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.