Solved
fauvarque.danielBest answer
ST Employee
Jul 23, 2024 11:09 AM UTC
As stated in the documentation if you provide an npz with the input and the output just use the --vi option
-vi/valinput |
indicates the custom test data set which must be used. If not defined an internal self-generated random data set is used (refer to [METRIC], “Input validation files” section) - Optional |
-vo/valoutput |
indicates the expected custom output values. If the data are already provided in a simple file ('*.npz') through the '-vi' option this argument is skipped - Optional |
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.