Skip to main content
GBrug.1
Associate
Nov 18, 2022 11:06 AM UTC
Solved

X-Cube-AI. AI_ERROR_CODE_LOCK during network creation.

I'm working on a ML project with X-Cube-AI version 7.3.0 with the STM32F4DISCOVERY board.

I created the neural network with tensorflow, and the analysis went smooth, the network occupies 25 kb of flash and 8 kb of ram.

This is the neural network summary;

Model: "sequential_8"
_________________________________________________________________
 Layer (type) Output Shape Param # 
=================================================================
 conv1d_10 (Conv1D) (None, 28, 16) 1456 
 
 batch_normalization_49 (Bat (None, 28, 16) 48 
 chNormalization) 
 
 conv1d_11 (Conv1D) (None, 28, 32) 1568 
 
 max_pooling1d_25 (MaxPoolin (None, 14, 32) 0 
 g1D) 
 
 batch_normalization_50 (Bat (None, 14, 32) 96 
 chNormalization) 
 
 conv1d_12 (Conv1D) (None, 14, 64) 6208 
 
 batch_normalization_51 (Bat (None, 14, 64) 192 
 chNormalization) 
 
 conv1d_13 (Conv1D) (None, 14, 64) 4160 
 
 max_pooling1d_26 (MaxPoolin (None, 7, 64) 0 
 g1D) 
 
 batch_normalization_52 (Bat (None, 7, 64) 192 
 chNormalization) 
 
 conv1d_14 (Conv1D) (None, 7, 14) 910 
 
 max_pooling1d_27 (MaxPoolin (None, 3, 14) 0 
 g1D) 
 
 batch_normalization_53 (Bat (None, 3, 14) 42 
 chNormalization) 
 
 flatten_8 (Flatten) (None, 42) 0 
 
 dense_2 (Dense) (None, 1) 43 
 
 batch_normalization_54 (Bat (None, 1) 3 
 chNormalization) 
 
 activation_8 (Activation) (None, 1) 0 
 
=================================================================
Total params: 14,918
Trainable params: 14,536
Non-trainable params: 382
_________________________________________________________________

However, at runtime when I call the function ai_network_create I obtain an error of tyoe 51 and code 65 which corresponds to AI_ERROR_CREATE_FAILED and to AI_ERROR_CODE_LOCK respectively.

What this code means? Why it happens?

	ai_handle network;
	ai_error err = ai_network_create(&network, (const ai_buffer*)AI_NETWORK_DATA_CONFIG);
	 if (err.type != AI_ERROR_NONE)
	 {
	 printf("E: AI error in NN creation - type=%d code=%d\r\n", err.type, err.code);
	 // TODO: error handling
	 }
	 else
	 {
	 printf("NN successfully created.\n");
	 }

This topic has been closed for replies.
jean-michel.dBest answer
ST Employee
Nov 18, 2022 2:58 PM UTC

Hi,

Before to call the ai_network_XX() fcts, the STM32 CRC IP should be enabled. This IP is used to check that the AI library is executed on a STM32 device.

The following HAL code is normally sufficent to enable and to clock the CRC IP.

 __HAL_RCC_CRC_CLK_ENABLE();

br,

JM

2 replies

jean-michel.dBest answer
ST Employee
Nov 18, 2022 2:58 PM UTC

Hi,

Before to call the ai_network_XX() fcts, the STM32 CRC IP should be enabled. This IP is used to check that the AI library is executed on a STM32 device.

The following HAL code is normally sufficent to enable and to clock the CRC IP.

 __HAL_RCC_CRC_CLK_ENABLE();

br,

JM

GBrug.1
GBrug.1Author
Associate
Nov 18, 2022 3:26 PM UTC

Thank you! This solved my problem.